This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: 4 port Store-and-Forward Switch by using 2 x Dual EMAC Switch of AM57xx

Part Number: AM5728

Tool/software: TI-RTOS

Hi,

I understood that it is difficult to implement 4 port EMAC Switch without PRU firmware modification.

---------------------------
The PRU firmware need to be modified. To avoid overloading the Host with FDB operations, the firmware Switch should perform FDB lookups and forward Layer 2 (L2) traffic. There is no FDB in current firmware.
----------------------------

If they don't need Cut Through Switch for 4ch, is it possible for them to implement 4ch Store-and-Forward Switch by using two of Dual EMAC Switch of AM57xx without PRU firmware modification ? 

Port 0                                                  |
            Cut Through available    |
Port 1                                                  |

                                                        Store-and-Forward Switch available ? 

Port 2                                                  |
            Cut Through available      |
Port 3                                                  |

Thanks and regards,
Hideaki