Part Number: AM5718
Tool/software: Linux
Hi,
SDK : ti-processor-sdk-linux-rt-am57xx-evm-05.00.00.15
Toolchain : ARM GCC 8.3 2019.03 hard-float toolchain
u-boot : u-boot-2018.01
-----------------------------------------------------------------------------------
The following problems occur when compiling the boot loader.
Do you know the cause?
LD lib/built-in.o
LD u-boot
/toolchain/bin/arm-linux-gnueabihf-ld.bfd: cmd/built-in.o: in function `print_cpu_list':
/sanion/RGBTest/bsp/u-boot-2018.01/cmd/cpu.c:35: undefined reference to `cpu_get_desc'
/toolchain/bin/arm-linux-gnueabihf-ld.bfd: /sanion/RGBTest/bsp/u-boot-2018.01/cmd/cpu.c:40: undefined reference to `cpu_get_info'
make[1]: *** [Makefile:1261: u-boot] error 1
make[1]: directory '/sanion/RGBTest/bsp/u-boot-2018.01' out
make: *** [Makefile:77: boot] error 2