This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6546: Temperature sensing

Part Number: AM6546


Hi all,

How to use the TEMP_DIODE_P Pin W6 for internal Temperature sensing for die temperature monitoring?.

Is there any external circuit required for using this?.

Regards

Tauseef Kazi

  • That pin is only for production testing. The AM65x family has three other sensors available spread evenly through the chip.

    If you're using Linux they're available by reading the thermal_zones temp value.

    cat /sys/class/thermal/thermal_zone*/temp

    I'm not sure if RTOS has a driver for it. See the VBGAPTS section of the AM65x TRM for more details if you're curious. 

  • You can also read these temperature sensors through CCS using the GEL scripts that are supplied through the chip support package.