This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6657: TMS320C6657 processor in TMDSEVM6657 is fixed point?

Part Number: TMDSEVM6657
Other Parts Discussed in Thread: TMS320C6657

Hello everyone,

I am working with TMDSEVM6657 evaluation board. I have ordered it through DigiKey. In the technical reference manual that I got inside the package that came with evaluation board I have found the information that the TMS320C6657 on evaluation board is fixed point. However, in a discussion with TI support, as well as inside the datasheets for this processor on TI site I have found the information that the processor is both fixed point and floating point.

Link to the evaluation board:

http://www.ti.com/tool/TMDSEVM6657

Does anyone can help me clarify this confusion?

I would appreciate any comment, suggestion or help.

Thank you in advance!

Kind regards,

Dejana

  • Hi, Dejana,

    I suspect it is the 3rd party manufacturer of the EVM misprinted the info. In all TI website on C6657, the fixed and floating point are mentioned, but in 3rd party manufacturer website, I see only fixed point is listed. You should be okay with the floating point feature.

    Rex

  • Hi Rex,

    Thank you very much! This very helpful.

    My idea is to try using some of the functions from floating point library. If they can be used, it is definitely both fixed point and floating point. 

    Kind regards,

    Dejana