Part Number: AM3354
Other Parts Discussed in Thread: TSC2046, ADS7846
Hi all,
I am using custom board with AM3354 SoC. Board is copy of BeagleBone Black + TSC2046 connected to SPI0 CS0 which is used for touchscreen controller of the AM-1024768FTMQW-T00H LCD.
I use Processor SDK Linux 06_01_00_08.
In order to get any response when I touch the display I had to modify the ads7846.c driver as shown bellow:
/*
* We'd set TX word size 8 bits and RX word size to 13 bits ... except
* that even if the hardware can do that, the SPI controller driver
* may not. So we stick to very-portable 8 bit words, both RX and TX.
*/
- spi->bits_per_word = 8;
+ spi->bits_per_word = 16;
- spi->mode = SPI_MODE_0;
+ spi->mode = SPI_MODE_1;
err = spi_setup(spi);
if (err < 0)
However, when I touch the display I start getting the following error outputted continuously:
[ 1487.869143] ads7846 spi0.0: spi_sync --> -22
[ 1487.889109] ads7846 spi0.0: spi_sync --> -22
[ 1487.909106] ads7846 spi0.0: spi_sync --> -22
[ 1487.929139] ads7846 spi0.0: spi_sync --> -22
[ 1487.949088] ads7846 spi0.0: spi_sync --> -22
[ 1487.969110] ads7846 spi0.0: spi_sync --> -22
[ 1487.989070] ads7846 spi0.0: spi_sync --> -22
[ 1488.009115] ads7846 spi0.0: spi_sync --> -22
[ 1488.029154] ads7846 spi0.0: spi_sync --> -22
Here is my dts node:
&spi0 {
pinctrl-names = "default";
pinctrl-0 = <&spi0_pins>;
status = "okay";
tsc2046@0 {
reg = <0>;
compatible = "ti,tsc2046";
interrupt-parent = <&gpio3>;
interrupts = <14 0>;
spi-max-frequency = <1000000>;
pendown-gpio = <&gpio3 14 0>;
ti,x-min = /bits/ 16 <0>;
ti,x-max = /bits/ 16 <8000>;
ti,y-min = /bits/ 16 <0>;
ti,y-max = /bits/ 16 <4800>;
ti,x-plate-ohms = /bits/ 16 <350>;
ti,pressure-max = /bits/ 16 <255>;
wakeup-source;
};
};
I seem to get the touchscreen controller registered & initialized in the kernel:
[ 4.327498] ads7846 spi0.0: spi0.0 supply vcc not found, using dummy regulator
[ 4.334991] ads7846 spi0.0: Linked as a consumer to regulator.0
[ 4.341408] ads7846 spi0.0: touchscreen, irq 55
[ 4.346128] input: ADS7846 Touchscreen as /devices/platform/ocp/48030000.spi/spi_master/spi0/spi0.0/0
I am able to see the gpio3_14 registered in /proc/interrupts as irq for ads7846:
52: 0 INTC 111 Level 48310000.rng
53: 965 INTC 37 Level SGX ISR
55: 0 481ae000.gpio 14 Edge ads7846
56: 0 44e07000.gpio 6 Edge 48060000.mmc cd
I see the irq incrementing when tapping on the display, but at the same time the kernel starts continously outputting ads7846 spi0.0: spi_sync --> -22, the part where this error comes from is:
ads7846_read_state() ->
while (msg_idx < ts->msg_count) {
ts->wait_for_sync();
m = &ts->msg[msg_idx];
error = spi_async(ts->spi, m);//error = spi_sync(ts->spi, m);
if (error) {
dev_err(&ts->spi->dev, "spi_async --> %d\n", error);
packet->tc.ignore = true;
return;
}
which can be tracked to spi.c driver, where spi_sync() is implemented. The error -22 seems to indicate that the message is of incompatible type (include/uapi/asm-generic/errno-base.h):
#define EINVAL 22 /* Invalid argument */
Also when ads7846 spi0.0: spi_sync --> -22, there is NO signal on the spi bus. The ads7846.c cannot read the touchscreen data from the TSC2046.
Previously I've used a customized driver with kernel 3.2 (Sitara Linux SDK 06.00.00.00) and it worked, but now the requirement is to stick with PROCESSOR SDK LINUX (kernel mainline) sources, so I have to use ads7846.c.
Can anyone help with pointers on what might be wrong?
Thanks and regards.