This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,expert
I read from the document "Jacito 7 LPDDR4 board design and layout guidelines" that on die capacitance information should be considered duriing ddr signal simulation. But I learned from TI FAE that TDA4 has no on-die capacitance. This makes me confused that if we should use the on die decoupling circuit value for simulation as below.
And the fact is there are on-die capacitance on DRAM side, and if we set no on-die decoupling value in simulation project for controller, the output DQ waveform would have a big amplitute(about 3V) for controller driver.
Please suggest how to deal with the on die information for TDA4 and would it be correct if the on-die capacitance value is used in simulaiton? Thanks