Hi,
we used AM3352,but i don't understand some places.
1.I don't understand OP100,OP50,OP120,Nitro,Turbo(please see red box), What do they mean?we don't know what we choosed
2.what is operating maximum current of AM3352 in 0--60℃?
3. when 1Ghz,maximum current is 1000mA, it is so high,but I understanding it is not so high,because Generally, the maximum LDO current is about 1A.,so LDO have a hard time satisfying the normal working of AM3352 ,TJ of AM3352 and LDO are very high. how to understand it?
4.Which I/O high level is 3.3V? and Which I/O high level is 1.5V? and Which I/O high level is 1.8V?
Thanks