Part Number: TMDSSK3358
Hi,
in attempting to build the am335x-evm-linux-06.03.00.106 software stack AND reflash the sd card using ./bin/create-sdcard.sh, I've blown the card and cannot get back to anything that boots at all.
is there a default image or instructions for the shipped 3-partition layout so that I can start over with this?
steps taken
1) dd the 3 partitions off the sd card to 3 local respective images. I think now that I should have taken a monolithic approach here and copied off the entire card in one image...
2. run make all from my <sdk-install> directory. seems to have gone well, didn't get any bail-out errors.
3. follow instructions for running ./bin/create-sdcard.sh
the questions about paths to <what ever> are very unclear, as are the instructions about it for copying custom builds. I never got the script to work and finish installing u-boot/kernel & rootfs because it incessantly complains about "file not found" sorts of problems, even though my input tab-completes track right down the directory/ies I THINK it's ask for.
4. So I locally mounted the original rootfs partition image taken from the sdcard in step 1.
I ran a recursive cp with preserve-links args, from the top of that mount point over to a fresh, empty sdcard. this did not boot the starter kit.
5. Reinitialzed/blanked the sdcard, and I ran dd of the original rootfs image onto a (once again) the blank sdcard. this did not boot the starter kit either.
which brings me here. I hope someone can give me nudge in the right direction.
thanks, -pete u.