Other Parts Discussed in Thread: DRA829,
Tool/software: TI C/C++ Compiler
My question is
When we plug the Realtek demo board into two PCIe slot, we would get the different results.
The software on SD card is the factory settings and the boot log is as attachment.
According to packet sniffing for PCIe, in slot 1, our demo board has started to transmit the TS2 packets when TI DRA829 EVM still transmit the TS1 packet.
The reason is maybe timeout or another. However in slot 2, it didn't happen.
So, we are confused by the results. Could anyone give me some advice?
In Slot 1:
We didn't get any information about PCIe client (Realtek demo board).
j7-evm login: root
root@j7-evm:~# lspci
0000:00:00.0 PCI bridge: Texas Instruments Device b00d
0001:00:00.0 PCI bridge: Texas Instruments Device b00d
0002:00:00.0 PCI bridge: Texas Instruments Device b00d
In Slot 2:
We got the information about PCIe client (Realtek demo board).
j7-evm login: root
root@j7-evm:~# lspci
0000:00:00.0 PCI bridge: Texas Instruments Device b00d
0001:00:00.0 PCI bridge: Texas Instruments Device b00d
0001:01:00.0 Ethernet controller: Realtek Semiconductor Co., Ltd. Device 906a
0001:01:00.1 Network controller: Realtek Semiconductor Co., Ltd. Device 906f
0002:00:00.0 PCI bridge: Texas Instruments Device b00d
U-Boot SPL 2019.01-g66126341c8 (Dec 11 2019 - 21:52:37 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.8.1-v2019.08b (Terrific Llam') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default environment Remoteproc 2 started successfully ** File not found /lib/firmware/j7-mcu-r5f0_0-fw ** Starting ATF on ARM64 core... NOTICE: BL31: v2.1(release):ti2019.02-rc4 NOTICE: BL31: Built : 21:52:04, Dec 11 2019 I/TC: I/TC: OP-TEE version: ti2019.02-89-ge5a8779-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Wed Dec 11 21:52:32 UTC 2019 aarch64 I/TC: Initialized U-Boot SPL 2019.01-g66126341c8 (Dec 11 2019 - 21:52:51 +0000) Detected: J7X-BASE-CPB rev E3 Detected: J7X-GESI-EXP rev E3 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 ti_sci_power_domain_on: get_device(91) failed (-19) U-Boot 2019.01-g66126341c8 (Dec 11 2019 - 21:52:51 +0000) SoC: J721E PG 1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM2-SOM rev E7 DRAM: 4 GiB Flash: 0 Bytes MMC: ti_sci_power_domain_on: get_device(91) failed (-19) sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... *** Warning - bad CRC, using default environment In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E3 Detected: J7X-GESI-EXP rev E3 Detected: J7X-VSC8514-ETH rev E2 Net: Warning: ethernet@046000000 using MAC address from ROM eth0: ethernet@046000000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 ** Unable to read file boot.scr ** 40 bytes read in 2 ms (19.5 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... 13338632 bytes read in 557 ms (22.8 MiB/s) 98400 bytes read in 5 ms (18.8 MiB/s) 3653 bytes read in 1 ms (3.5 MiB/s) ## Flattened Device Tree blob at 82000000 Booting using the fdt blob at 0x82000000 Loading Device Tree to 00000000fdda6000, end 00000000fdec1fff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080] [ 0.000000] Linux version 4.19.73-g0cabba2b47 (oe-user@oe-host) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 SMP PREEMPT Wed Dec 11 21:54:17 UTC 2019 [ 0.000000] Machine model: Texas Instruments K3 J721E SoC [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] bootconsole [ns16550a0] enabled [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 63 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a4000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a4100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a5000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a5100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a6000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa100000, size 63 MiB [ 0.000000] OF: reserved mem: initialized node c66-memory@a6100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ae000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a7000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ae100000, size 31 MiB [ 0.000000] OF: reserved mem: initialized node c66-memory@a7100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node c71-dma-memory@a8000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b0100000, size 127 MiB [ 0.000000] OF: reserved mem: initialized node c71-memory@a8100000, compatible id shared-dma-pool [ 0.000000] cma: Reserved 512 MiB at 0x00000000c0000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.1 [ 0.000000] random: get_random_bytes called from start_kernel+0x94/0x3e4 with crng_init=0 [ 0.000000] percpu: Embedded 2 pages/cpu s52632 r8192 d70248 u131072 [ 0.000000] Detected PIPT I-cache on CPU0 [ 0.000000] CPU features: enabling workaround for EL2 vector hardening [ 0.000000] Speculative Store Bypass Disable mitigation not required [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 58438 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),-@8m(ospi.rootfs);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs) root=PARTUUID=41a1b097-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes) [ 0.000000] Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes) [ 0.000000] software IO TLB: mapped [mem 0xf9da0000-0xfdda0000] (64MB) [ 0.000000] Memory: 3127808K/3743744K available (8510K kernel code, 738K rwdata, 3136K rodata, 576K init, 642K bss, 91648K reserved, 524288K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=2. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: no VLPI support, no direct LPI support [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8c0800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GIC: using LPI property table @0x00000008c00a0000 [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000 [ 0.000000] CPU0: using LPI pending table @0x00000008c00b0000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008347] Console: colour dummy device 80x25 [ 0.012900] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023569] pid_max: default: 32768 minimum: 301 [ 0.028309] Security Framework initialized [ 0.032512] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes) [ 0.039367] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes) [ 0.070701] ASID allocator initialised with 32768 entries [ 0.084227] rcu: Hierarchical SRCU implementation. [ 0.097169] Platform MSI: gic-its@1820000 domain created [ 0.102697] PCI/MSI: /interconnect@100000/interrupt-controller@1800000/gic-its@1820000 domain created [ 0.120132] smp: Bringing up secondary CPUs ... [ 0.157031] Detected PIPT I-cache on CPU1 [ 0.157046] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000 [ 0.157074] CPU1: using LPI pending table @0x00000008c0310000 [ 0.157096] CPU1: Booted secondary processor 0x0000000001 [0x411fd080] [ 0.157138] smp: Brought up 1 node, 2 CPUs [ 0.184974] SMP: Total of 2 processors activated. [ 0.189784] CPU features: detected: GIC system register CPU interface [ 0.196366] CPU features: detected: 32-bit EL0 Support [ 0.201849] CPU: All CPU(s) started at EL2 [ 0.206035] alternatives: patching kernel code [ 0.210996] devtmpfs: initialized [ 0.218671] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.228633] futex hash table entries: 512 (order: -1, 32768 bytes) [ 0.235338] pinctrl core: initialized pinctrl subsystem [ 0.241005] NET: Registered protocol family 16 [ 0.245887] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____)) [ 0.253451] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.262620] DMA: preallocated 256 KiB pool for atomic allocations [ 0.275958] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.282811] HugeTLB registered 512 MiB page size, pre-allocated 0 pages [ 0.290204] cryptd: max_cpu_qlen set to 1000 [ 0.295037] vsys_3v3: supplied by evm_12v0 [ 0.299300] vsys_5v0: supplied by evm_12v0 [ 0.303828] SCSI subsystem initialized [ 0.307876] media: Linux media interface: v0.10 [ 0.312510] videodev: Linux video capture interface: v2.00 [ 0.318124] pps_core: LinuxPPS API ver. 1 registered [ 0.323193] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.332530] PTP clock support registered [ 0.336539] EDAC MC: Ver: 3.0.0 [ 0.340334] Advanced Linux Sound Architecture Driver Initialized. [ 0.346866] clocksource: Switched to clocksource arch_sys_counter [ 0.353156] VFS: Disk quotas dquot_6.6.0 [ 0.357202] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes) [ 0.366610] NET: Registered protocol family 2 [ 0.371311] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes) [ 0.379362] TCP established hash table entries: 32768 (order: 2, 262144 bytes) [ 0.386846] TCP bind hash table entries: 32768 (order: 3, 524288 bytes) [ 0.393907] TCP: Hash tables configured (established 32768 bind 32768) [ 0.400636] UDP hash table entries: 2048 (order: 0, 65536 bytes) [ 0.406818] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes) [ 0.413487] NET: Registered protocol family 1 [ 0.418155] RPC: Registered named UNIX socket transport module. [ 0.424208] RPC: Registered udp transport module. [ 0.429012] RPC: Registered tcp transport module. [ 0.433815] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.440629] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 0.450262] Initialise system trusted keyrings [ 0.454881] workingset: timestamp_bits=46 max_order=16 bucket_order=0 [ 0.462850] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.469001] NFS: Registering the id_resolver key type [ 0.474170] Key type id_resolver registered [ 0.478441] Key type id_legacy registered [ 0.482539] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.489439] 9p: Installing v9fs 9p2000 file system support [ 0.496536] Key type asymmetric registered [ 0.500723] Asymmetric key parser 'x509' registered [ 0.505725] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.513284] io scheduler noop registered [ 0.517290] io scheduler deadline registered [ 0.521688] io scheduler cfq registered (default) [ 0.526495] io scheduler mq-deadline registered [ 0.531121] io scheduler kyber registered [ 0.535986] pinctrl-single 4301c000.pinmux: 94 pins, size 376 [ 0.542069] pinctrl-single 11c000.pinmux: 173 pins, size 692 [ 0.548209] pinctrl-single a40000.timesync_router: 512 pins, size 2048 [ 0.557101] ti-pat 31010000.pat: Found PAT Rev 1.0 with 16384 pages [ 0.563523] ti-pat 31010000.pat: Failed to create 31010000.pat debugfs directory [ 0.571182] ti-pat 31011000.pat: Found PAT Rev 1.0 with 16384 pages [ 0.577594] ti-pat 31011000.pat: Failed to create 31011000.pat debugfs directory [ 0.585224] ti-pat 31012000.pat: Found PAT Rev 1.0 with 16384 pages [ 0.591636] ti-pat 31012000.pat: Failed to create 31012000.pat debugfs directory [ 0.599268] ti-pat 31013000.pat: Found PAT Rev 1.0 with 2048 pages [ 0.605589] ti-pat 31013000.pat: Failed to create 31013000.pat debugfs directory [ 0.613215] ti-pat 31014000.pat: Found PAT Rev 1.0 with 2048 pages [ 0.619537] ti-pat 31014000.pat: Failed to create 31014000.pat debugfs directory [ 0.628398] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.639533] brd: module loaded [ 0.645289] loop: module loaded [ 0.649529] libphy: Fixed MDIO Bus: probed [ 0.653867] tun: Universal TUN/TAP device driver, 1.6 [ 0.659259] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k [ 0.667265] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.673330] sky2: driver version 1.30 [ 0.677606] VFIO - User Level meta-driver version: 0.3 [ 0.683189] i2c /dev entries driver [ 0.687175] sdhci: Secure Digital Host Controller Interface driver [ 0.693490] sdhci: Copyright(c) Pierre Ossman [ 0.698122] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.704335] ledtrig-cpu: registered to indicate activity on CPUs [ 0.711146] optee: probing for conduit method from DT. [ 0.716407] optee: revision 3.6 (e5a8779a) [ 0.716507] optee: initialized driver [ 0.725119] NET: Registered protocol family 17 [ 0.729720] 9pnet: Installing 9P2000 support [ 0.734097] Key type dns_resolver registered [ 0.738647] registered taskstats version 1 [ 0.742831] Loading compiled-in X.509 certificates [ 0.752063] ti-sci 44083000.dmsc: ABI: 2.6 (firmware rev 0x0013 '19.8.1-v2019.08b (Terrific Llam') [ 0.776890] random: fast init done [ 0.816552] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 100 kHz [ 0.822480] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz [ 0.828428] omap_i2c 42120000.i2c: bus 2 rev0.12 at 100 kHz [ 0.834440] pca953x 3-0020: 3-0020 supply vcc not found, using dummy regulator [ 0.841846] pca953x 3-0020: Linked as a consumer to regulator.0 [ 0.871402] pca953x 3-0022: 3-0022 supply vcc not found, using dummy regulator [ 0.878812] pca953x 3-0022: Linked as a consumer to regulator.0 [ 0.885685] GPIO line 481 (MCASP/TRACE_MUX_S0) hogged as output/low [ 0.892409] GPIO line 482 (MCASP/TRACE_MUX_S1) hogged as output/high [ 0.898972] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz [ 0.904961] omap_i2c 2010000.i2c: bus 4 rev0.12 at 400 kHz [ 0.910827] omap_i2c 2020000.i2c: bus 5 rev0.12 at 100 kHz [ 0.916732] pca953x 6-0020: 6-0020 supply vcc not found, using dummy regulator [ 0.924133] pca953x 6-0020: Linked as a consumer to regulator.0 [ 0.951529] GPIO line 464 (CODEC_RSTz) hogged as output/high [ 0.957441] omap_i2c 2030000.i2c: bus 6 rev0.12 at 400 kHz [ 0.963299] omap_i2c 2040000.i2c: bus 7 rev0.12 at 100 kHz [ 0.969146] omap_i2c 2050000.i2c: bus 8 rev0.12 at 100 kHz [ 0.975060] pca953x 9-0020: 9-0020 supply vcc not found, using dummy regulator [ 0.982461] pca953x 9-0020: Linked as a consumer to regulator.0 [ 1.011288] omap_i2c 2060000.i2c: bus 9 rev0.12 at 400 kHz [ 1.025608] cdns-dp-phy 5050000.serdes: 4 lanes, max bit rate 5.400 Gbps [ 1.033720] cdns-pcie-host d000000.pcie: missing "mem" [ 1.039309] cdns-pcie-host d000000.pcie: Linked as a consumer to phy-5000000.serdes.0 [ 2.048685] cdns-pcie-host d000000.pcie: Phy link never came up [ 2.054739] cdns-pcie-host d000000.pcie: host bridge /interconnect@100000/pcie@2900000/pcie@d000000 ranges: [ 2.064710] cdns-pcie-host d000000.pcie: IO 0x10001000..0x10010fff -> 0x10001000 [ 2.072541] cdns-pcie-host d000000.pcie: MEM 0x10011000..0x17ffffff -> 0x10011000 [ 2.080426] cdns-pcie-host d000000.pcie: PCI host bridge to bus 0000:00 [ 2.087188] pci_bus 0000:00: root bus resource [bus 00-0f] [ 2.092794] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x10001000-0x10010fff]) [ 2.102484] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff] [ 2.109534] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 2.119404] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 2.129295] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x92 may corrupt adjacent RW1C bits [ 2.139256] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xb2 may corrupt adjacent RW1C bits [ 2.149244] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x84 may corrupt adjacent RW1C bits [ 2.160892] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 2.169080] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 2.179040] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 2.188999] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits [ 2.198958] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x6 may corrupt adjacent RW1C bits [ 2.210390] pci_bus 0000:00: 1-byte config write to 0000:00:00.0 offset 0x1a may corrupt adjacent RW1C bits [ 2.220358] pci 0000:00:00.0: PCI bridge to [bus 01] [ 2.225735] cdns-pcie-host d800000.pcie: missing "mem" [ 2.231392] cdns-pcie-host d800000.pcie: Linked as a consumer to phy-5010000.serdes.1 [ 3.240765] cdns-pcie-host d800000.pcie: Phy link never came up [ 3.246818] cdns-pcie-host d800000.pcie: host bridge /interconnect@100000/pcie@2910000/pcie@d800000 ranges: [ 3.256785] cdns-pcie-host d800000.pcie: IO 0x18001000..0x18010fff -> 0x18001000 [ 3.264616] cdns-pcie-host d800000.pcie: MEM 0x18011000..0x1fffffff -> 0x18011000 [ 3.272492] cdns-pcie-host d800000.pcie: PCI host bridge to bus 0001:00 [ 3.279253] pci_bus 0001:00: root bus resource [bus 00-0f] [ 3.284859] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x18001000-0x18010fff]) [ 3.294727] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff] [ 3.303443] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 3.313213] pci 0001:00:00.0: PCI bridge to [bus 01] [ 3.318546] cdns-pcie-host e000000.pcie: missing "mem" [ 3.324134] cdns-pcie-host e000000.pcie: Linked as a consumer to phy-5020000.serdes.2 [ 4.333507] cdns-pcie-host e000000.pcie: Phy link never came up [ 4.339559] cdns-pcie-host e000000.pcie: host bridge /interconnect@100000/pcie@2920000/pcie@e000000 ranges: [ 4.349526] cdns-pcie-host e000000.pcie: IO 0x4400001000..0x4400010fff -> 0x00001000 [ 4.357712] cdns-pcie-host e000000.pcie: MEM 0x4400011000..0x4407ffffff -> 0x00011000 [ 4.365943] cdns-pcie-host e000000.pcie: PCI host bridge to bus 0002:00 [ 4.372704] pci_bus 0002:00: root bus resource [bus 00-0f] [ 4.378309] pci_bus 0002:00: root bus resource [io 0x20000-0x2ffff] (bus address [0x1000-0x10fff]) [ 4.387556] pci_bus 0002:00: root bus resource [mem 0x4400011000-0x4407ffffff] (bus address [0x00011000-0x07ffffff]) [ 4.399986] pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 4.409724] pci 0002:00:00.0: PCI bridge to [bus 01] [ 4.415191] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235 [ 4.425065] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled [ 4.431824] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64 [ 4.439506] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211 [ 4.449646] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled [ 4.456405] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64 [ 4.464018] omap8250 40a00000.serial: PM domain pd:149 will not be powered off [ 4.471525] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 7, base_baud = 6000000) is a 8250 [ 4.480628] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 19, base_baud = 3000000) is a 8250 [ 4.489364] console [ttyS2] enabled [ 4.489364] console [ttyS2] enabled [ 4.496397] bootconsole [ns16550a0] disabled [ 4.496397] bootconsole [ns16550a0] disabled [ 4.505284] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 20, base_baud = 3000000) is a 8250 [ 4.514071] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 21, base_baud = 3000000) is a 8250 [ 4.522789] arm-smmu-v3 36600000.smmu: ias 48-bit, oas 48-bit (features 0x00001faf) [ 4.531528] arm-smmu-v3 36600000.smmu: msi_domain absent - falling back to wired irqs [ 4.541098] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled [ 4.551611] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled [ 4.561764] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled [ 4.572005] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled [ 4.582805] scsi host0: ufshcd [ 4.596751] cadence-qspi 47040000.spi: mt35xu512aba (65536 Kbytes) [ 4.602930] 7 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 4.609529] Creating 7 MTD partitions on "47040000.spi.0": [ 4.612341] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[1, 1], lane[1, 1], pwr[SLOWAUTO_MODE, SLOWAUTO_MODE], rate = 0 [ 4.615002] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 4.633047] 0x000000080000-0x000000280000 : "ospi.tispl" [ 4.638542] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 4.644109] 0x000000680000-0x0000006a0000 : "ospi.env" [ 4.649434] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 4.652981] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[3, 3], lane[2, 2], pwr[FAST MODE, FAST MODE], rate = 2 [ 4.666841] cdns-ufshcd 4e84000.ufs: ufshcd_find_max_sup_active_icc_level: Regulator capability was not set, actvIccLevel=0 [ 4.678084] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 4.678145] scsi 0:0:0:49488: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6 [ 4.683584] 0x000000800000-0x000004000000 : "ospi.rootfs" [ 4.697328] scsi 0:0:0:49476: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6 [ 4.706080] cdns-ufshcd 4e84000.ufs: ufshcd_scsi_add_wlus: BOOT WLUN not found [ 4.814949] cadence-qspi 47040000.spi: Cadence QSPI NOR probe failed -517 [ 4.822445] cadence-qspi 47050000.spi: n25q512a (65536 Kbytes) [ 4.842960] cadence-qspi 47050000.spi: Cadence QSPI NOR probe failed -517 [ 4.850208] am65-cpsw-nuss 46000000.ethernet: rx-flow-id-base is not set -22 [ 4.857259] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 [ 4.868672] UDMA has not been proped [ 4.872246] am65-cpsw-nuss 46000000.ethernet: Failed to request tx dma channel -517 [ 4.880650] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0 [ 4.889089] mmc0: Unknown controller version (4). You may experience problems. [ 4.896332] mmc0: CQHCI version 5.10 [ 4.930604] mmc0: SDHCI controller on 4f80000.sdhci [4f80000.sdhci] using ADMA 64-bit [ 4.944395] vdd_mmc1: supplied by vsys_3v3 [ 4.948903] pca953x 4-0020: 4-0020 supply vcc not found, using dummy regulator [ 4.956137] pca953x 4-0020: Linked as a consumer to regulator.0 [ 4.983532] GPIO line 448 (DP0_PWR_SW_EN) hogged as output/high [ 4.990134] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100 [ 4.997016] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100 [ 5.003941] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100 [ 5.010887] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100 [ 5.017762] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100 [ 5.025499] mmc0: Command Queue Engine enabled [ 5.029940] mmc0: new HS400 MMC card at address 0001 [ 5.035253] mmcblk0: mmc0:0001 S0J56X 14.8 GiB [ 5.040021] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB [ 5.046174] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB [ 5.052158] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (242:0) [ 5.332674] ti-udma 285c0000.udmap: Channels: 24 (tchan: 48, echan: 0, rchan: 48, rflow: 96) [ 5.342240] ti-udma 31150000.udmap: Channels: 84 (tchan: 140, echan: 160, rchan: 140, rflow: 300) [ 5.354407] cadence-qspi 47040000.spi: mt35xu512aba (65536 Kbytes) [ 5.360590] 7 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 5.367189] Creating 7 MTD partitions on "47040000.spi.0": [ 5.372664] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 5.378388] 0x000000080000-0x000000280000 : "ospi.tispl" [ 5.383902] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 5.389474] 0x000000680000-0x0000006a0000 : "ospi.env" [ 5.394806] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 5.400721] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 5.406198] 0x000000800000-0x000004000000 : "ospi.rootfs" [ 5.413707] cadence-qspi 47050000.spi: n25q512a (65536 Kbytes) [ 5.421406] am65-cpsw-nuss 46000000.ethernet: rx-flow-id-base is not set -22 [ 5.428460] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 [ 5.445853] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 5.456225] pps pps0: new PPS source ptp1 [ 5.460314] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:1 [ 5.469257] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 0.4 [ 5.476463] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 5.518874] am65-cpsw-nuss 46000000.ethernet: davinci mdio revision 9.7, bus freq 1000000 [ 5.527035] libphy: 46000000.ethernet: probed [ 5.532610] sdhci-am654 4fb0000.sdhci: Linked as a consumer to regulator.4 [ 5.539493] sdhci-am654 4fb0000.sdhci: Linked as a consumer to regulator.5 [ 5.546381] mmc1: Unknown controller version (4). You may experience problems. [ 5.553625] mmc1: CQHCI version 5.10 [ 5.587428] mmc1: SDHCI controller on 4fb0000.sdhci [4fb0000.sdhci] using ADMA 64-bit [ 5.604545] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 5.611456] hctosys: unable to open rtc device (rtc0) [ 5.637196] vdd_mmc1: disabling [ 5.640341] ALSA device list: [ 5.643302] No soundcards found. [ 5.646911] Waiting for root device PARTUUID=41a1b097-02... [ 6.984242] mmc1: new ultra high speed DDR50 SDHC card at address aaaa [ 6.991283] mmcblk1: mmc1:aaaa SL16G 14.8 GiB [ 7.005896] mmcblk1: p1 p2 [ 7.184192] EXT4-fs (mmcblk1p2): recovery complete [ 7.189564] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) [ 7.197656] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 7.206997] devtmpfs: mounted [ 7.210094] Freeing unused kernel memory: 576K [ 7.214545] Run /sbin/init as init process [ 7.372211] systemd[1]: System time before build time, advancing clock. [ 7.428094] NET: Registered protocol family 10 [ 7.432875] Segment Routing with IPv6 [ 7.453645] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 7.475078] systemd[1]: Detected architecture arm64. Welcome to Arago 2019.09! [ 7.506230] systemd[1]: Set hostname to <j7-evm>. [ 7.605236] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling. [ 7.622279] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.) [ 7.728343] random: systemd: uninitialized urandom read (16 bytes read) [ 7.738279] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 7.754916] random: systemd: uninitialized urandom read (16 bytes read) [ 7.761657] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 7.778909] random: systemd: uninitialized urandom read (16 bytes read) [ 7.786061] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 7.802915] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 7.829205] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. Mounting POSIX Message Queue File System... Starting Load Kernel Modules... [ 7.869497] cmemk: loading out-of-tree module taints kernel. [ 7.876052] CMEMK module: reference Linux version 4.19.73 [ 7.881720] no physical memory specified Mounting Huge Pages File System... [ 7.886350] cmemk initialized Starting Journal Service... [ 7.902679] cryptodev: driver 1.9 loaded. [ OK ] Listening on udev Control Socket. [ OK ] Reached target Swap. [ OK ] Listening on Network Service Netlink Socket. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Listening on udev Kernel Socket. Starting udev Coldplug all Devices... [ OK ] Created slice system-getty.slice. [ OK ] Reached target Remote File Systems. [ OK ] Listening on initctl Compatibility Named Pipe. Mounting Temporary Directory (/tmp)... Starting Remount Root and Kernel File Systems... [ OK ] Started Forward Password Requests to Wall Di[ 8.075918] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null) rectory Watch. Mounting Kernel Debug File System... [ OK ] Reached target Paths. [ OK ] Listening on Process Core Dump Socket. [ OK ] Created slice system-serial\x2dgetty.slice. Starting Create list of required st…ce nodes for the current kernel... [ OK ] Started Journal Service. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Started Load Kernel Modules. [ OK ] Mounted Huge Pages File System. [ OK ] Mounted Temporary Directory (/tmp). [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Mounted Kernel Debug File System. [ OK ] Started Create list of required sta…vice nodes for the current kernel. Starting Create Static Device Nodes in /dev... Mounting Kernel Configuration File System... Starting Apply Kernel Variables... Starting Flush Journal to Persistent Storage... [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Started udev Coldplug all Devices. [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Apply Kernel Variables. [ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... Mounting /media/ram... [ OK ] Reached target Containers. Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. [ OK ] Mounted /media/ram. [ 8.491380] systemd-journald[150]: Received request to flush runtime journal from PID 1 Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. [ OK ] Started udev Kernel Device Manager. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Load/Save Random Seed. Starting Create Volatile Files and Directories... [ OK ] Started Create Volatile Files and Directories. Starting Network Service... Starting Update UTMP about System Boot/Shutdown... Starting Network Time Synchronization... [ OK ] Started Network Service. [ 8.669129] pcm3168a 6-0044: Linked as a consumer to regulator.2 [ OK ] Found device /dev/ttyS2. [ 8.687009] pcm3168a 6-0044: Linked as a consumer to regulator.3 Starting Wait for Network to be Configured... Starting Network Name Resolution... [ OK ] Started Update UTMP about System Boot/Shutdown. [ 8.743602] img_enc 4200000.video-encoder: vxe_init_mem: adding heap of type 1 [ 8.764825] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node c66-dma-memory@a7000000 [ 8.768784] img_enc 4200000.video-encoder: vxe_init_mem: using heap 1 for internal alloc [ OK ] Started Network Time Synchronization. [ 8.798958] k3-dsp-rproc 4d80800000.dsp: configured DSP for remoteproc mode [ OK ] Reached target System Initialization. [ 8.808575] img_dec 4300000.video-decoder: decoder registered as /dev/video0 Starting Reboot and dump vmcore via kexec... [ 8.840160] iommu: Adding device 0000:00:00.0 to group 0 [ 8.850315] pci-endpoint-test 0000:00:00.0: of_irq_parse_pci: failed with rc=-22 [ 8.857753] k3-dsp-rproc 4d80800000.dsp: local reset is deasserted for device [ 8.857947] img_enc 4200000.video-encoder: encoder registered as /dev/video1 [ OK ] Listening on dropbear.socket. [ 8.875085] remoteproc remoteproc0: 4d80800000.dsp is available [ 8.879428] pci_generic_config_write32: 29 callbacks suppressed [ 8.879432] pci_bus 0000:00: 1-byte config write to 0000:00:00.0 offset 0x3c may corrupt adjacent RW1C bits [ 8.887388] remoteproc remoteproc0: Direct firmware load for j7-c66_0-fw failed with error -2 [ OK ] Started Daily Cleanup of Temporary Directorie[ 8.911066] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node c66-dma-memory@a6000000 s. [ 8.922695] remoteproc remoteproc0: powering up 4d80800000.dsp [ 8.928790] remoteproc remoteproc0: Direct firmware load for j7-c66_0-fw failed with error -2 [ OK ] Listening on RPCbind Server Activation Socket[ 8.938188] remoteproc remoteproc0: request_firmware failed: -2 . [ 8.953544] k3-dsp-rproc 4d81800000.dsp: configured DSP for remoteproc mode [ 8.953657] iommu: Adding device 0001:00:00.0 to group 1 [ 8.967152] k3-dsp-rproc 4d81800000.dsp: local reset is deasserted for device [ 8.974347] pci-endpoint-test 0001:00:00.0: of_irq_parse_pci: failed with rc=-22 [ 8.981889] pci_bus 0001:00: 1-byte config write to 0001:00:00.0 offset 0x3c may corrupt adjacent RW1C bits [ 8.993800] remoteproc remoteproc1: 4d81800000.dsp is available [ 8.999820] remoteproc remoteproc1: Direct firmware load for j7-c66_1-fw failed with error -2 [ 9.008708] k3-dsp-rproc 64800000.dsp: assigned reserved memory node c71-dma-memory@a8000000 [ 9.017215] remoteproc remoteproc1: powering up 4d81800000.dsp [ 9.023069] remoteproc remoteproc1: Direct firmware load for j7-c66_1-fw failed with error -2 [ 9.031899] remoteproc remoteproc1: request_firmware failed: -2 [ 9.037832] k3-dsp-rproc 64800000.dsp: configured DSP for remoteproc mode [ OK ] Listening on D-Bus System Message Bus Socket.[ 9.046291] iommu: Adding device 0002:00:00.0 to group 2 [ 9.056931] remoteproc remoteproc2: 64800000.dsp is available [ 9.062782] pci-endpoint-test 0002:00:00.0: of_irq_parse_pci: failed with rc=-22 [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activati[ 9.070947] remoteproc remoteproc2: Direct firmware load for j7-c71_0-fw failed with error -2 on Socket. [ 9.090068] remoteproc remoteproc2: powering up 64800000.dsp [ OK ] Reached target Sockets. [ 9.097474] pci_bus 0002:00: 1-byte config write to 0002:00:00.0 offset 0x3c may corrupt adjacent RW1C bits [[ 9.110090] remoteproc remoteproc2: Direct firmware load for j7-c71_0-fw failed with error -2 OK ] Reached target Basic System. [ 9.118699] remoteproc remoteproc2: request_firmware failed: -2 [ 9.132752] tidss 4a00000.dss: dispc7_wb_find_free_ovr: found ovr vp2 (1) [ 9.140748] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ OK ] Started System Logging Service. [ 9.155309] [drm] No driver support for vblank timestamp query. [ OK ] Started irqbalance daemon. [ 9.170940] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 0 Starting Print notice about GPLv3 packages... [ 9.182639] [drm] Cannot find any crtc or sizes [ 9.197781] [drm] Cannot find any crtc or sizes [ 9.205159] ntb_hw_epf 0000:00:00.0: of_irq_parse_pci: failed with rc=-22 [ OK ] Started Kernel Logging Service. [ OK ] Started D-Bus System Message Bus. [ OK ] Started Periodic Command Scheduler. [ OK ] Started Job spooling tools. Starting rc.pvr.service... [ 9.243105] pci_bus 0000:00: 1-byte config write to 0000:00:00.0 offset 0x3c may corrupt adjacent RW1C bits [ 9.257214] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 9.274030] ntb_hw_epf 0000:00:00.0: Cannot set DMA mask [ 9.280447] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 9.291220] ntb_hw_epf 0000:00:00.0: Failed to init PCI Starting RPC Bind Service... Starting Login Service... [ OK ] Started TEE Supplicant. [ OK ][ 9.305149] ntb_hw_epf: probe of 0000:00:00.0 failed with error -5 Reached target System Time Synchronized. [ 9.317933] ntb_hw_epf 0001:00:00.0: of_irq_parse_pci: failed with rc=-22 [ 9.329062] pci_bus 0001:00: 1-byte config write to 0001:00:00.0 offset 0x3c may corrupt adjacent RW1C bits [ 9.340132] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits [ 9.350973] ntb_hw_epf 0001:00:00.0: Cannot set DMA mask [ OK ] Started Daily rotation of log files. [ OK ] Reached target Timers. [ OK ] Started Network Name Resolution. [ OK ] Started Reboot an[ 9.372640] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits d dump vmcore via kexec. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Reached target Host and Network Name[ 9.390776] ntb_hw_epf 0001:00:00.0: Failed to init PCI Lookups. [ OK ] Reached target Network. [ 9.402102] ntb_hw_epf: probe of 0001:00:00.0 failed with error -5 Starting Permit User Sessions... [ 9.402322] k3_r5_rproc interconnect@100000:interconnect@28380000:r5fss@41000000: creating child devices for R5F cores [ 9.412168] ntb_hw_epf 0002:00:00.0: of_irq_parse_pci: failed with rc=-22 [ 9.442648] pci_bus 0002:00: 1-byte config write to 0002:00:00.0 offset 0x3c may corrupt adjacent RW1C bits [ 9.467929] ntb_hw_epf 0002:00:00.0: Cannot set DMA mask [ 9.475241] platform 41000000.r5f: configured R5F for remoteproc mode [ 9.477296] ntb_hw_epf 0002:00:00.0: Failed to init PCI [ 9.493772] ntb_hw_epf: probe of 0002:00:00.0 failed with error -5 [ 9.534946] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000 [ 9.544085] remoteproc remoteproc3: 41000000.r5f is available [ 9.554647] pvrsrvkm 4e20000000.gpu: Linked as a consumer to genpd:0:4e20000000.gpu [ 9.561611] remoteproc remoteproc3: Direct firmware load for j7-mcu-r5f0_0-fw failed with error -2 [ 9.565342] pvrsrvkm 4e20000000.gpu: Linked as a consumer to genpd:1:4e20000000.gpu [ 9.574880] remoteproc remoteproc3: powering up 41000000.r5f [ 9.587470] remoteproc remoteproc3: Direct firmware load for j7-mcu-r5f0_0-fw failed with error -2 [ 9.588030] PVR_K: 327: Read BVNC 22.104.208.318 from HW device registers [ 9.596498] remoteproc remoteproc3: request_firmware failed: -2 [ 9.606289] k3_r5_rproc interconnect@100000:r5fss@5c00000: creating child devices for R5F cores [ 9.618137] PVR_K: 327: RGX Device initialised with BVNC 22.104.208.318 [ 9.627618] [drm] Initialized pvr 1.10.5371573 20170530 for 4e20000000.gpu on minor 1 [ 9.640903] platform 5c00000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [ 9.658848] platform 5c00000.r5f: configured R5F for IPC-only mode [ 9.672781] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a2000000 [ 9.685641] remoteproc remoteproc4: 5c00000.r5f is available [ 9.694921] platform 5d00000.r5f: configured R5F for remoteproc mode [ 9.703709] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000 [ 9.719778] remoteproc remoteproc5: 5d00000.r5f is available [ 9.733973] k3_r5_rproc interconnect@100000:r5fss@5e00000: creating child devices for R5F cores [ 9.756042] TI DP83867 k3-cpsw-mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=k3-cpsw-mdio:00, irq=POLL) [ 9.772094] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 9.779585] platform 5e00000.r5f: configured R5F for remoteproc mode [ 9.803343] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000 [ 9.819787] remoteproc remoteproc4: powering up 5c00000.r5f [ 9.825477] remoteproc remoteproc4: Booting fw image j7-main-r5f0_0-fw, size 1416996 [ OK ] Started Login Service.[ 9.835025] remoteproc remoteproc6: 5e00000.r5f is available [ 9.843667] platform 5c00000.r5f: R5F core initialized in IPC-only mode [ OK ] Started RPC Bind Service. [ 9.851168] virtio_rpmsg_bus virtio0: rpmsg host is online [ OK ] Started Permit User Sessions. [ 9.862936] remoteproc remoteproc4: registered virtio0 (type 7) [ OK ] Found device /dev/ttyS1. [ 9.874009] remoteproc remoteproc4: remote processor 5c00000.r5f is now up [ 9.886980] virtio_rpmsg_bus virtio0: creating channel rpmsg-kdrv addr 0x1a [ 9.899205] rpmsg-kdrv-eth-switch rpmsg-kdrv-2-mpu_1_0_ethswitch-device-0: Device info: permissions: 007FFFFF uart_id: 2 [ 9.910245] remoteproc remoteproc5: powering up 5d00000.r5f [ 9.915837] remoteproc remoteproc5: Booting fw image j7-main-r5f0_1-fw, size 2179860 [ 9.928975] rpmsg-kdrv-eth-switch rpmsg-kdrv-2-mpu_1_0_ethswitch-device-0: FW ver 0.1 (rev 1) 21/Oct/2019 SHA:beff669b [ 9.939903] remoteproc remoteproc5: erroneous trace resource entry [ 9.948025] remoteproc remoteproc5: Failed to process resources: -22 [ 9.958362] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2 [ 9.972020] remoteproc remoteproc6: powering up 5e00000.r5f [ 9.980668] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2 [ OK ] Started rc.pvr.service. [ 9.997467] remoteproc remoteproc6: request_firmware failed: -2 [ OK ] Started Avahi mDNS/DNS-SD Stack. Starting weston.service... [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Reached target Login Prompts. Starting Synchro[ 10.106935] j721e-audio sound@0: pcm3168a-dac <-> 2ba0000.mcasp mapping ok nize System and HW clocks... [ OK ] Started NFS status monitor for NFSv2/3 locking.. [FAILED] Failed to start Synchronize System and HW clocks. See 'systemctl status sync-clocks.service' for details. [ OK ] Started weston.service. Starting telnetd.service... [ 10.161733] j721e-audio sound@0: pcm3168a-adc <-> 2ba0000.mcasp mapping ok [ OK ] Started telnetd.service. [ 10.176411] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0: virt_cpsw_nuss mac loaded [ 10.187373] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0: rdev_features:00000003 rdev_mtu:1522 flow_id:172 tx_psil_dst_id:4A00 [ 10.204766] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0: local_mac_addr:00:00:00:00:00:00 rdev_mac_addr:70:ff:76:1d:9f:70 Starting thttpd.service... [ OK ] Started thttpd.service. [ 10.604004] cdns-usb3 6000000.usb: DRD version v1 (ID: 0004024e, rev: 00000200) [ 10.627933] omap_rng 4e10000.trng: Random Number Generator ver. 241b34c [ 10.628260] random: crng init done [ 10.657480] random: 7 urandom warning(s) missed due to ratelimiting [ 10.715720] cdns-usb3 6400000.usb: DRD version v1 (ID: 0004024e, rev: 00000200) Starting Save/Restore Sound Card State... [ 10.764588] remoteproc remoteproc7: b034000.pru is available [ 10.773598] pru-rproc b034000.pru: PRU rproc node pru@b034000 probed successfully [ 10.799413] remoteproc remoteproc8: b004000.rtu is available [ 10.806276] pru-rproc b004000.rtu: PRU rproc node rtu@b004000 probed successfully [ 10.807968] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down [ 10.815190] remoteproc remoteproc9: b00a000.txpru is available [ 10.825792] pru-rproc b00a000.txpru: PRU rproc node txpru@b00a000 probed successfully [ 10.846453] remoteproc remoteproc10: b038000.pru is available [ 10.858640] pru-rproc b038000.pru: PRU rproc node pru@b038000 probed successfully [ 10.866587] remoteproc remoteproc11: b006000.rtu is available [ 10.872416] pru-rproc b006000.rtu: PRU rproc node rtu@b006000 probed successfully [ 10.880366] remoteproc remoteproc12: b00c000.txpru is available [ 10.886603] pru-rproc b00c000.txpru: PRU rproc node txpru@b00c000 probed successfully [ 10.894858] remoteproc remoteproc13: b134000.pru is available [ 10.900926] pru-rproc b134000.pru: PRU rproc node pru@b134000 probed successfully [ 10.908868] remoteproc remoteproc14: b104000.rtu is available [ 10.914959] pru-rproc b104000.rtu: PRU rproc node rtu@b104000 probed successfully [ 10.922828] remoteproc remoteproc15: b10a000.txpru is available [ 10.929056] pru-rproc b10a000.txpru: PRU rproc node txpru@b10a000 probed successfully [ 10.937405] remoteproc remoteproc16: b138000.pru is available [ 10.943492] pru-rproc b138000.pru: PRU rproc node pru@b138000 probed successfully [ 10.951450] remoteproc remoteproc17: b106000.rtu is available [ 10.957571] pru-rproc b106000.rtu: PRU rproc node rtu@b106000 probed successfully [ 10.965444] remoteproc remoteproc18: b10c000.txpru is available [ 10.971644] pru-rproc b10c000.txpru: PRU rproc node txpru@b10c000 probed successfully [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ 11.016950] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0: virt_cpsw_nuss mac started [ 11.054037] usbcore: registered new interface driver usbfs [ 11.059610] usbcore: registered new interface driver hub [ 11.065011] usbcore: registered new device driver usb [ 11.109172] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 11.114778] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1 [ 11.126199] xhci-hcd xhci-hcd.2.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000000000010010 [ 11.135996] xhci-hcd xhci-hcd.2.auto: irq 324, io mem 0x06410000 [ 11.142457] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19 [ 11.150883] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 11.158256] usb usb1: Product: xHCI Host Controller [ 11.163374] usb usb1: Manufacturer: Linux 4.19.73-g0cabba2b47 xhci-hcd [ 11.170099] usb usb1: SerialNumber: xhci-hcd.2.auto [ 11.175325] hub 1-0:1.0: USB hub found [ 11.179581] hub 1-0:1.0: 1 port detected [ 11.184042] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 11.189829] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2 [ 11.197796] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed [ 11.204775] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 11.213168] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19 [ 11.221687] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 11.229119] usb usb2: Product: xHCI Host Controller [ 11.234162] usb usb2: Manufacturer: Linux 4.19.73-g0cabba2b47 xhci-hcd [ 11.240847] usb usb2: SerialNumber: xhci-hcd.2.auto [ 11.246094] hub 2-0:1.0: USB hub found [ 11.250322] hub 2-0:1.0: 1 port detected [ OK ] Found device /dev/mmcblk1p1. Starting File System Check on /dev/mmcblk1p1... [ OK ] Started File System Check on /dev/mmcblk1p1. Mounting /run/media/mmcblk1p1... [ OK ] Mounted /run/media/mmcblk1p1. [ 11.518895] usb 1-1: new high-speed USB device number 2 using xhci-hcd [ 11.671171] usb 1-1: New USB device found, idVendor=0451, idProduct=8142, bcdDevice= 1.00 [ 11.679442] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1 [ 11.686643] usb 1-1: SerialNumber: 40000849DE36 [ 11.691646] hub 1-1:1.0: USB hub found [ 11.695464] hub 1-1:1.0: 4 ports detected [ OK ] Started Save/Restore Sound Card State. [ OK ] Reached target Sound Card. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf bash-dev bash bc binutils cifs-utils coreutils-dev coreutils cpio cpp-symlinks cpp dosfstools elfutils g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gettext glmark2 gstreamer1.0-libav gzip libbfd libcairo-perf-utils libdw1 libelf1 libgdbm-compat4 libgdbm-dev libgdbm6 libgettextlib libgettextsrc libgmp-dev libgmp10 libgmpxx4 libidn2-0 libmpc3 libmpfr6 libreadline-dev libreadline7 libunistring2 m4-dev m4 make nettle parted which If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove <package> Where <package> is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ OK ] Started Print notice about GPLv3 packages. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org j7-evm ttyS2 Arago 2019.09 j7-evm ttyS2 j7-evm login: root root@j7-evm:~#