This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question on a PCI connector resistor

Anonymous
Anonymous

Hello,

 

I have one question on a connection on EVM6437.

 

On its PCI connector, I found that B3 GND is connected to VCC_3V3 rather than ground, and there is a NO-POP placeholder R164 connected with B3. Most important is that B3’s net PCI_PLUGn is then used to control {PCI_DETECTn & PCIEN} signal.

     

 

  

 

Is this configuration something like a pulling-up? When there is no PCI device connected, B3 will be pulled up by VCC_3V3 to high, thus effectively making

PCI_DETECTn

H

PCIEN

L

 

On the other hand, if a PCI device is connected, B3 will be connected through the device to other GND pins and has voltage low, making

PCI_DETECTn

H

PCIEN

L

 

So it is indeed provide DETECT and ENABLE functionality as the associated signal names suggest.

 

So in this regard R163 is essentially a pull-up?

 

 

 

 

 

Thanks,

Zheng