Hello,
Board : Beaglebone Black
Linux SDK version : ti-processor-sdk-linux-am335x-evm-06.03.00.106
u-boot SPL version : U-Boot SPL 2019.01-gc148924-dirty
u-boot version : U-Boot 2019.01-gc148924-dirty
With the u-boot images from ti-processor-linux-sdk on Beaglebone Black ,
I frequently encounter the "###ERROR###Please RESET the board### " (console output is below) message.
The RESET button should be manually pressed couple of times to boot the board normally.
How do I overcome this scenario ?? Kindly advice.
Regards,
Adarsh
-------------------------------------------------------------------------
U-Boot SPL 2019.01-gc148924-dirty (Oct 08 2020 - 06:47:09 +0530)
Trying to boot from MMC1
spl: mmc init failed with error: -524
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
U-Boot SPL 2019.01-gc148924-dirty (Oct 08 2020 - 06:47:09 +0530)
Trying to boot from MMC1
spl: mmc init failed with error: -524
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
U-Boot SPL 2019.01-gc148924-dirty (Oct 08 2020 - 06:47:09 +0530)
Trying to boot from MMC1
spl: mmc init failed with error: -524
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
U-Boot SPL 2019.01-gc148924-dirty (Oct 08 2020 - 06:47:09 +0530)
Trying to boot from MMC1
U-Boot 2019.01-gc148924-dirty (Oct 08 2020 - 06:47:09 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM335x BeagleBone Black
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from FAT... <ethaddr> not set. Validating first E-fuse MC
Net: eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in ROM is de:ad:be:ef:00:01
Address in environment is 04:79:b7:ad:02:20
, eth1: usb_ether
Hit any key to stop autoboot: 0
=>
----------------------------------------------------