Other Parts Discussed in Thread: PRU-CGT
Hello, I am new to bare metal programming but I'm hoping to create a bare metal application with FreeRTOS on the beaglebone black using both pru and gpio. I plan to cross compile from Debian 10. I have 2 question that I hope someone can help me with.
- Is the pru-cgt compiler(www.ti.com/.../PRU-CGT-2-1) a bare-metal/freestanding compiler? And can I use it from my host linux machine to cross compile for beaglebone as the target?
- I understand that pru-cgt can compile c/asm code written for the pru but can it also compile code written for the gpio on P8 and P9 headers? Ill be using the ti starter ware for AM335x to write code for the gpio and the pru support package to program the pru
Also i want to avoid JTAG related hardware, thank you.