This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMOMAPL138B-HIREL: Data routing between HPI port and the DDR2 controller using DMA and its timing

Part Number: SMOMAPL138B-HIREL

Dear TI Experts,

We are planning to send around 68K samples of data from the HPI port to the DSP. Is there any DMA option inside the DSP which can route the data sent to HPI port from external host to the DDR2 controller? Essentially the data has to be written to DDR2 memory from the external host through HPI port.

Regards,

Jonard Rico