This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Clarification on dev-boot mode

Part Number: TDA4VM


Hi TI,

The TRM says in chapter 4.3.3 the following about Dev-boot:

Q1: Does that mean, that DMSC ROM code is executed as if this was a normal boot? (Configuring PLLs)

Q2: Is R5 ROM Code also executed? (Configuring Power and Resource Management)

Q3: If connecting the board to CCS debug session using dev-boot, do I need to execute launch.js script? Or is the necessary config (PLLs, RM, PM) already done by DMSC/R5 ROM Code?

Thanks for clarification and best regards,

Felix

  • Hi,

    Apologies this was in a wrong state. What is the exact use case here? Do you want to run some use case using dev-boot mode?
    Can you add more details?

    - Keerthy

  • Hi Keerthy,

    thanks for your reply. The basic use case is to reduce the time it takes to connect the TDA4VM to a CCS Debug session (Currently this takes about 3 min and is done via Blackhawk XDS560v2 Debugger on Linux VM and the default launch.js script provided by TI). As a first approach, I wanted to avoid the launch.js + GEL functions, since parts of this config are already done by the ROM codes (DMSC,R5) and SPL/SBL. Please correct me, if this is a wrong assumption.

    This is where dev-boot mode comes in. Since DMSC ROM Code + R5 ROM Code are doing part of the configurations, which are done by the launch.js script (in connection with the OnTargetConnect() GEL function), in specific configuring PLLs and PSCs, I thought, that starting from this point I can load applications to mcu2_0 or other cores (Maybe it is necessary to start SPL/SBL on mcu1_0 first). See also this thread in e2e: https://e2e.ti.com/support/processors/f/processors-forum/993957/tda4vm-about-dmsc-rom-code-and-r5-rom-code).

    Thanks and best regards,

    Felix

  • Felix,

    Then can you just boot to u-boot prompt and then attach. If you do not want to go through the entire 3 minutes. U-boot comes up in few seconds
    and you can connect to R5 or the A72 cores. Will that work for you?

    - Keerthy

  • Hi Keerthy,

    Hmm, I already tried that, but CCS throws errors, when I try to connect to MCU2_0, MCU2_1, MCU3_0, MCU3_1:

    "Error connecting to the target:
    (Error -1170 @ 0x0)
    Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
    (Emulation package 9.2.0.00002)"

    Unfortunately, the proposed solutions (power cycle, JTAG settings) do not work.

    My setup: I try to boot from SD card with unmodified boot files. So also the default firmware in lib/firmware, which gets loaded to the R5s are untouched. The Target Configuration File is without the GEL file for the DMSC, because this config is done by SPL and ROM Code I think.

    I also got one additional question: Is TDA4VM, when halted at U-Boot prompt, in a smiliar state as it would be after running launch.js in No-Boot Mode? Are there any differences in configuring PLLs or PSCs?

    Thanks again for your help and best regards,

    Felix

  • Hi Keerthy,

    I could solve the issue. It seemed, that MCU2_0 had to be started first in U-Boot in order to connect to it.

    Thanks and best regards,

    Felix

  • Great! Thanks for updating the ticket. I am closing this.

    - Keerthy