This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
The TRM says in chapter 4.3.3 the following about Dev-boot:
Q1: Does that mean, that DMSC ROM code is executed as if this was a normal boot? (Configuring PLLs)
Q2: Is R5 ROM Code also executed? (Configuring Power and Resource Management)
Q3: If connecting the board to CCS debug session using dev-boot, do I need to execute launch.js script? Or is the necessary config (PLLs, RM, PM) already done by DMSC/R5 ROM Code?
Thanks for clarification and best regards,
Felix
Hi Keerthy,
thanks for your reply. The basic use case is to reduce the time it takes to connect the TDA4VM to a CCS Debug session (Currently this takes about 3 min and is done via Blackhawk XDS560v2 Debugger on Linux VM and the default launch.js script provided by TI). As a first approach, I wanted to avoid the launch.js + GEL functions, since parts of this config are already done by the ROM codes (DMSC,R5) and SPL/SBL. Please correct me, if this is a wrong assumption.
This is where dev-boot mode comes in. Since DMSC ROM Code + R5 ROM Code are doing part of the configurations, which are done by the launch.js script (in connection with the OnTargetConnect() GEL function), in specific configuring PLLs and PSCs, I thought, that starting from this point I can load applications to mcu2_0 or other cores (Maybe it is necessary to start SPL/SBL on mcu1_0 first). See also this thread in e2e: https://e2e.ti.com/support/processors/f/processors-forum/993957/tda4vm-about-dmsc-rom-code-and-r5-rom-code).
Thanks and best regards,
Felix
Felix,
Then can you just boot to u-boot prompt and then attach. If you do not want to go through the entire 3 minutes. U-boot comes up in few seconds
and you can connect to R5 or the A72 cores. Will that work for you?
- Keerthy
Hi Keerthy,
Hmm, I already tried that, but CCS throws errors, when I try to connect to MCU2_0, MCU2_1, MCU3_0, MCU3_1:
"Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.2.0.00002)"
Unfortunately, the proposed solutions (power cycle, JTAG settings) do not work.
My setup: I try to boot from SD card with unmodified boot files. So also the default firmware in lib/firmware, which gets loaded to the R5s are untouched. The Target Configuration File is without the GEL file for the DMSC, because this config is done by SPL and ROM Code I think.
I also got one additional question: Is TDA4VM, when halted at U-Boot prompt, in a smiliar state as it would be after running launch.js in No-Boot Mode? Are there any differences in configuring PLLs or PSCs?
Thanks again for your help and best regards,
Felix