hello all,
can any one plz send me the block diagram of TMS320C6452. also i want to know that for full duplex communication, will both rj45 works in parallel or not?
is there two MAC controller IC's?
waiting for reply...
regards
adnan khurshid
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello all,
can any one plz send me the block diagram of TMS320C6452. also i want to know that for full duplex communication, will both rj45 works in parallel or not?
is there two MAC controller IC's?
waiting for reply...
regards
adnan khurshid
The functional block diagrams are now available on the product folders as a graphic. Just click to enlarge. The detailed diagram is in the datasheet and both are located here http://focus.ti.com/docs/prod/folders/print/tms320c6452.html
I am unable to answer your other questions, perhaps another community member may be able to jump in.
Mike
The C6452 EVM includes two separate PHYs meaning that both ports can be used independently. I believe that the NDK (TCP/IP Stack) v2.0 and above will provide the software support for operating both simultaneously.adnan khurshid said:can any one plz send me the block diagram of TMS320C6452. also i want to know that for full duplex communication, will both rj45 works in parallel or not?
is there two MAC controller IC's?
hello Tim; can you plz help me in finding the exact location or say function in the ndk example helloworld under evm648 folder. i have spent lot of time on it, i have seen packet buffer addresses but i want to change them and then transmit through LAN. i am recieving LAN packets through ethernet ports.
regards
adnan