Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hi, Experts,
Please give us your comments for the unexpected behavior which customer found like below.
- Create the Master Task on Core0
- Create the task_T0 on Core0
- Create the task_T1 Core1
- Create Suspend Clock 3 ms and Resume Clock 100 ms in the TI Clock class.
- Start Suspend Clock and Resume Clock in the TI Clock class.
- After 3ms : Interrupt START
- Task_setPri(Task T0, -1)
- Task_setPri(Task T1, -1)
-> This Task_setPri is Never return (looks hung-up)
Customer summarized them as PDF and I attached it here.
2500.task.pdf
In addition to this, this behavior was also happened on behavior on TMDXIDK5728. Here is the customer's project.
1643.LC_rtos_clk_not_timeout_app_am572x_a15_1024.zip
If you have any questions, please let me know.
Best regards.
Kaka