Hi,
I have the same problem as this post:
https://e2e.ti.com/support/processors/f/791/t/534394?tisearch=e2e-sitesearch&keymatch=reboot
For some reason, I need to reset SMPS and LDO during linux reboot.
We have followed the AM5728 reference design and the reset outn pin is connected to the PMIC NRESWARM pin.
When rebooting, I can see the PMIC NRESWARM and RESET_OUT asserted low then asserted high, but LMPS and LDO's power state never be toggled or changed.
WR_S bit in the SMPSx_CTRL register or the LDOx_CTRL register is 0, and MODE_ACTIVE bit is 0x3(Forced PWM).
How do I reset the voltage of LMPS and LDO?
Thanks,
allen