This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950EVM: TI_204C_IP VIVADO error

Part Number: AFE7950EVM

Tool/software:

Hi.

I am working with AFE7950EVM and TI JESD IP at Vivado 2021.1.

The example I am referring to is "ZCU102_AFE79XX_8b10b_10Gbps".

My goal is to change parameter(Line Rate 9.8Gbps, LMFS 8421, RXTX)  in the example to (Line Rate 10Gbps, LMFS 4841, TX).

I changed jesd_link_params.vh, TI_204c_IP_ref.sv and etc

NUMBER_OF_R/TX_LANES 8 -> 4

NUMBER_OF_QUADS 2-> 1

LANE_ADC/DAC_TO_GT_MAP {4,5,6,7,3,0,2,1,} -> {3,0,2,1}

R/TX_LANE_DATA_WIDTH 64->32

R/TX_F_VAL 2->4

R/TX_K_VAL 32->16

PARAM_TX_M 4->8 in TI_204c_IP.sv

Accordingly, sys_pll, gth_8b10b_xcvr and xdc were modified.

However, during the bitgeneration process, an error as shown in the attached image occurs

what should i do to fix it

Regards