Hi ,
I have browsed the forum to look for a minimal example which uses an x degrees beamwidth for one single frame using all the 3 antennas. I think this is frame-based beam steering
It turned out that there are several examples for the BPM mode but not for the phase shifter settings. My confusion is there are many places to change but there is no way for me to verify I'm doing this correctly. Appreciate it any explanations for this.
1 st attempt. Phase Shifter in sensor Config.
I have followed the following formula the below document to generate the phase shift values for +20 degrees and put them into the Phase Shifter in sensor Config.
2nd attempt. BPM config tab
Here I have tried the same formula but divided it by 5.625. I wanted all the chirps in the frame to have this configuration.
Q1: First thing is I don't see much SNR gain for the objects in 20 degrees compared with TDM-MIMO. Am I doing something wrong?
Q2: Is there a way to get the beam width, I assume 20 degrees is the boresight angle.
Q3: What changes need to be done for the signal processing pipeline when it comes to AoA estimation to calculate azimuth and elevation angle?
Q4: What will be the angle resolution in this mode?
Thank You!
Isura