Dear Expert
For FDC2214:
1. Our application only considers single-channel Mode, so subsequent related issues are also discussed in single-channel Mode.
2. We pay most attention to the response time (the time between the input change and the data transmission from IIC to MCU) and ENOB
1. In single-channel mode, the time of Amplitude Correction is not reflected in the data manual. Please help to ask whether this value can be checked.
2. In single-channel mode, the VALID fREFx RANGE should be less than 35MHz. If 40MHz crystal oscillator is used externally, should the value of fREFx be adjusted actively or set automatically inside the chip?
3. How to calculate the response time more accurately in single-channel mode?
The way I think about it is:
(1) Sensor Activation Time
(2) Conversion Time
(3) Amplitude Correction Time(We don't know)
(4) IIC Transition Time of 28bit data (limited to 400kHz)
4. How is ENOB calculated?
Data sheet for FDC2214
That is
It can be deduced as:
Where did this value come from?
5. In addition, ENOB in the upper computer interface of FDC2214 is as follows:
The corresponding derivation is as follows:
And where did this value come from?
6. In addition, the manual of the chip calls itself 28bit. How did you get this?