Dear TI Support,
I am planning on using the CSI2 interface on AWR2243 to transfer ADC data, however I am unsure about the format used to transfer the data on the CSI2 interface.
The following document section 5.1 mentions that the data is sent on the CSI2 in RAW8/ RAW12/ RAW14 formats.
The following document fig 9-4 and 9-5 shows how the data is transferred over CSI2.
However I can't find an explanation of how the ADC data is mapped to the CSI2 RAW8/ RAW12/ RAW14 formats as specified in the MIPI specification.
So would you be able to point me to information that explains how the ADC data is mapped to the CSI2 RAW8/RAW12/RAW14 data formats across the 4 physical CSI2 data lanes? If you can provide an example mapping that would be most helpful.
Yours faithfully,
Jonathan Jones