Hi,
I use DCA1000 EVM to collect raw data from IWR 1443Boost. Set up works fine and I am able to capture RAW ADC data using mmWave Studio. Thereafter, I send commands using the RtttNetClientAPI.dll and MATLAB, which also works fine. I am able to capture the raw data files by sending the commands this way.
However, I noticed that the size of the .bin file that is produced by sending the commands through MATLAB is not consistent for different runs (Note all configuration parameters are kept the same). Whereas, (with the same configuration) the mmWave studio produces the same size files for different runs.
I will be really thankful if you can explain why this inconsistency is happening.