This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIC12400QDCPRQ1

Hi,

One of product design, requirement for digital inputs sensing, the following TI IC using for sensing,

 Part No : TIC12400QDCPRQ1

 

Requirements :

 Input Voltage Range : 0V to 16V DC

DI Type :  Active High and Low Signals.

No of channels : 13 No’s

 Here is the design circuit, the input resistor R146 value how to select? 

Thank you.

Regards.

Gopala