Hi Mr.David,
I am having some doubts in FDC1004 CAPDAC and FDC Configuration Register.
1.FDC1004 CAPDAC:
For Eg: capacitance: 90.237pF and CAPDAC: 75pF then i changed CAPDAC to 87.5 but capacitance which I have got is 116.697pF again I changed CAPDAC to 84.375pF and capacitance is 84.668pF(I tested in real time).
What I have understood in CAPDAC, it is used for setting offset capacitance and if offset is 10pF then I can able to measure capacitance between 10 to 26pF. If the capacitance is below or above the range then I am getting 26pF. Can you please tell me how CAPDAC is working in real time scenario.
2. FDC Configuration Register:
Every time before reading the capacitance I am checking the configuration register(0x0C-3rd bit) ready state. Sometimes I am not getting the ready state, once the FDC1004 went to this state then it will not comes to normal state, after words I am not able to read the capacitance till power RESET or FDC1004 RESET. Can you please tell me when this scenario will occurs and how to avoid this issue. Unknowingly i sent these information to your mail, sorry for the inconvenient. Here after i will follow TI Forum.
Thanks & Regards,
Suresh Kumar.S