Other Parts Discussed in Thread: IWR6843
Hello All,
We are working on custom antenna design using IWR6843 EVM ODS board, I have run the antenna simulations in HFSS tool attached the results as PPt, If any one can verify that the results attached IWR6843_60GHz ODS_HFSS Simu.pptx. I need to know why the Beam pattern has a split in the bore sight, also the combined total of the 4 RX antenna elements Gain should be by theoretically above 12dBi, but I have obtained gain aroud 10dBi in the entire band.
I have taken the Stack up/PCB material RO3003, 5mils thickness, with appropriate Cu thickness, followed the same board stack up, material, antenna dimensions are exactly 1:1 of TI, Wish to know the simulation results that I have got are correct or not.
IWR6843_60GHz ODS_HFSS Simu.pptx
I