This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: Initialization

Part Number: OPT3101

Is there a more concise document depicted register settings and order for monoshot mode.  We have followed what we could hack from the SDK, the datashaeet and some app notes but when trigger monoshot mode, the monoshot bit never returns to zero indicated measurement complete.  tg_en bit is shown in the data sheet to be set before anything else (figure 14) but we have seen in it in differing orders other places.

  • Hi Kirby,

    We do not have a specific monoshot document. Have you used the configurator tool to generate the monoshot mode configuration you are using? Have you set the device to trigger from the register or from the pin?

    Best,

    Alex

  • Yes triggering from monoshot bit.  I noticed that this bit needs to be set the TG enabled then I see the data ready signal on GPIO1.  How to perform another measurement is eluding me in addition to the monoshot bit never clearing.

    Here is configurator output I coded against.

    /*
    Copyright (c) 2018 Texas Instruments Incorporated
    All rights reserved not granted herein.
    Limited License.
    Texas Instruments Incorporated grants a world-wide, royalty-free, non-exclusive license under copyrights and patents it now or hereafter owns or controls to make, have made, use, import, offer to sell and sell ("Utilize") this software subject to the terms herein. With respect to the foregoing patent license, such license is granted solely to the extent that any such patent is necessary to Utilize the software alone. The patent license shall not apply to any combinations which include this software, other than combinations with devices manufactured by or for TI (TI Devices). No hardware patent is licensed hereunder.
    Redistributions must preserve existing copyright notices and reproduce this license (including the above copyright notice and the disclaimer and (if applicable) source code license limitations below) in the documentation and/or other materials provided with the distribution
    Redistribution and use in binary form, without modification, are permitted provided that the following conditions are met:
    * No reverse engineering, decompilation, or disassembly of this software is permitted with respect to any software provided in binary form.
    * any redistribution and use are licensed by TI for use only with TI Devices.
    * Nothing shall obligate TI to provide you with source code for the software licensed and provided to you in object code.
    If software source code is provided to you, modification and redistribution of the source code are permitted provided that the following conditions are met:
    * any redistribution and use of the source code, including any resulting derivative works, are licensed by TI for use only with TI Devices.
    * any redistribution and use of any object code compiled from the source code and any resulting derivative works, are licensed by TI for use only with TI Devices.
    Neither the name of Texas Instruments Incorporated nor the names of its suppliers may be used to endorse or promote products derived from this software without specific prior written permission.
    DISCLAIMER.
    THIS SOFTWARE IS PROVIDED BY TI AND TI's LICENSORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL TI AND TI'S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    */


    #include "OPT3101device.h"


    /* OPT3101 device initialization Sequence Header file written by OPT3101 Calibration tool - Version 0.9.1
    By: kirby.dotson
    On: 2019-10-14 20:10:10
    Configuration Settings:
    {
    "TXDCCurrent": 0,
    "LEDOrder": 131586,
    "superHDRMode": false,
    "genDeviceEEPROMConnection": false,
    "genDeviceI2CMasterConnection": 0,
    "autoHDRMode": false,
    "toolVersion": 0.9.1,
    "multiLEDMode": true,
    "monoshotMode": true,
    "genDeviceAmbientSupport": 0,
    "TX0HCurrent": 0,
    "monoshotModePowerupDelay": 153,
    "crc": 1304774340,
    "user": kirby.dotson,
    "genDeviceAvgFrameCount": 0,
    "timeStamp": 2019-10-14 20:09:55,
    "freqComp": false,
    "monoshotModeDeepSleep": false,
    "monoshotModeNFramesPerShot": 1,
    }
    */
    void OPT3101::device::initialize(void){
    // List of registers to initialize OPT3101 device after power-up

    this->reg.force_en_slave = 1; // //Since I2C Master bus is floating this register needs to be set to enable device to respond

    this->reg.tg_ovl_window_start = 7000; // //Overload flab observation window
    this->reg.en_temp_conv = 1; // //Enables the internal

    this->reg.clip_mode_fc = 1; // //Enables Clip mode for Frequency correction
    this->reg.clip_mode_temp = 0; // //Disables Clip mode for Temp coff phase correction
    this->reg.clip_mode_offset = 0; // //Disables Clip mode for phase offset correction
    this->reg.iq_read_data_sel = 3; // //Enables 16 bit frame counter
    this->reg.iamb_max_sel = 0; // //Sets maximum ambient support
    this->reg.en_temp_corr = 1; // //Enables Temperature Correction
    this->reg.gpio1_obuf_en=1; // //Enabled output buffer on GPIO1 pin
    this->reg.gpo1_mux_sel=2; // //select dig_gpo_0 on gpio1
    this->reg.dig_gpo_sel0 = 9; // //Select Data Ready on dig_gpo_0

    this->reg.monoshot_mode=3; // //Sets monoshot mode
    this->reg.dis_glb_pd_refsys=1; // Disables deep sleep PWRDN for blocks
    //this->reg.dis_glb_pd_temp_sens=1;
    //this->reg.dis_glb_pd_illum_drv=1
    //this->reg.dis_glb_pd_afe=1;
    //this->reg.dis_glb_pd_afe_dac=1;
    this->reg.dis_glb_pd_amb_dac=1;
    this->reg.dis_glb_pd_amb_adc=1;
    this->reg.dis_glb_pd_osc=1;
    //this->reg.dis_glb_pd_i2chost_osc=1;
    this->reg.MONOSHOT_NUMFRAME=1; // //Sets number of frames to me measured per trigger
    this->reg.powerup_delay=95; // //Power-up delay for every monoshot trigger

    this->reg.num_sub_frames = 0; // //Sub frames count
    this->reg.num_avg_sub_frames = 0; // //Average frames count
    this->reg.xtalk_filt_time_const = 10; // //Crosstalk filter time constant
    this->reg.tg_seq_int_start = 9850; // //Sequence Start
    this->reg.tg_seq_int_end = 9858; // //Sequence End
    this->reg.tg_seq_int_mask_start = 0; // //Same as AvgFrame Count
    this->reg.tg_seq_int_mask_end = 0; // //Same as AvgFrame Count

    this->reg.illum_dac_h_tx0 = 31; // //High Current settings [173.6mA:5.6mA X 31]
    this->reg.illum_scale_h_tx0 = 0; // //Illum scale for H [173.6mA:5.6mA X 31]

    this->reg.sel_hdr_mode = 1; // //Selecting H Channel by default

    this->reg.tx_seq_reg = 2184; // //Setting TX Switching order
    this->reg.en_tx_switch = 1 ; // //Enable TX Switching order

    this->reg.tg_en = 1; // //Enables Timing Generator

    this->configurationFlags_xtalkFilterTau = 10; // //This is not a register but a settings flag for the SDK
    this->configurationFlags_monoshotMode = true; // //This is not a register but a settings flag for the SDK
    this->configurationFlags_xtalkSettlingOneTauInMilliSeconds = 256; // //This is not a register but a settings flag for the SDK
    this->configurationFlags_xtalkSettlingOneTauInDataReadyCounts = 1024; // //This is not a register but a settings flag for the SDK
    this->configurationFlags_frameTimeInMilliSeconds = 1; // //This is not a register but a settings flag for the SDK
    this->configurationFlags_avgFrameCountExponentOfTwo = 0; // //This is not a register but a settings flag for the SDK

    }

    OPT3101::device::device(void):
    configurationFlags_isTXChannelActive{true,false,false},
    configurationFlags_isRegisterSetActive{false,true} {}

    OPT3101::calibrationC::calibrationC(void) : calibrationC(true) {
    this->recordLength = 1; // //This configuration requires 1 crosstalk and other configuration record(s)
    this->registerAddressListSize= 17; // //This configuration requires 17 registers [544] bits to be stored for calibration
    this->EEPROM_connected = false; // //This configuration helps configure EEPROM
    this->extTempSensor_connected= true; // //This configuration helps configure Ext temp sensor
    this->registerAddressList[0] = 0x31; // //Address for register(s) iphase_xtalk_reg_hdr1_tx0
    this->registerAddressList[1] = 0x32; // //Address for register(s) qphase_xtalk_reg_hdr1_tx0
    this->registerAddressList[2] = 0x5e; // //Address for register(s) temp_coeff_xtalk_iphase_hdr1_tx0
    this->registerAddressList[3] = 0x60; // //Address for register(s) temp_coeff_xtalk_qphase_hdr1_tx0
    this->registerAddressList[4] = 0x51; // //Address for register(s) phase_offset_hdr1_tx0,temp_coeff_illum_hdr1_tx0
    this->registerAddressList[5] = 0x48; // //Address for register(s) tmain_calib_hdr1_tx0,tillum_calib_hdr1_tx0
    this->registerAddressList[6] = 0x2d; // //Address for register(s) temp_coeff_main_hdr1_tx0
    this->registerAddressList[7] = 0x52; // //Address for register(s) temp_coeff_illum_hdr1_tx0
    this->registerAddressList[8] = 0x2e; // //Address for register(s) illum_xtalk_reg_scale
    this->registerAddressList[9] = 0x3a; // //Address for register(s) scale_temp_coeff_xtalk
    this->registerAddressList[10] = 0x71; // //Address for register(s) shift_illum_phase
    this->registerAddressList[11] = 0x43; // //Address for register(s) en_phase_corr,en_temp_corr,scale_phase_temp_coeff
    this->registerAddressList[12] = 0xb5; // //Address for register(s) scale_amb_phase_corr_coeff
    this->registerAddressList[13] = 0x0c; // //Address for register(s) amb_phase_corr_pwl_coeff0
    this->registerAddressList[14] = 0xb4; // //Address for register(s) amb_phase_corr_pwl_coeff1,amb_phase_corr_pwl_coeff2,amb_phase_corr_pwl_coeff3
    this->registerAddressList[15] = 0xb8; // //Address for register(s) amb_phase_corr_pwl_x0,amb_phase_corr_pwl_x1
    this->registerAddressList[16] = 0xb9; // //Address for register(s) amb_phase_corr_pwl_x2

    }