I want to design IR Sensor using OPT3101. Is distance value will be available on I2C
or is there any need to set registers.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to design IR Sensor using OPT3101. Is distance value will be available on I2C
or is there any need to set registers.
Hi,
Distance is read from I2C and yes OPT3101 needs to be configured and calibrated before data can be read. Please see here for our collateral on OPT3101
https://e2e.ti.com/support/sensors/f/1023/t/815766
Also want to confirm OPT3101 is a time of flight distance sensor. It can use IR light to do this, but it is not an IR light sensor in the sense that it is not an IR light intensity sensor.
Best,
Alex
Does OPT3101 needs two supply 1.8V and 3.3V for operating.
Is it ok to interface OPT3101 with 8051 microcontroller instead of MSP430F55031RGZ used in OPT3101 Evaluation Module.
Hi,
OPT3101 has internal LDO mode that allows single supply option. Yes, OPT3101 can work with any MCU with I2C.
Best,
Alex
Yes we have a lot of resources for OPT3101 including a full SDK which can act as firmware for reading data, configuring, and also performing calibration. Please see here for full list of resources.
Best,
Alex