This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Using mmWavestudio 2.0.1.000 occur error message "Timeout Error! System disconnected"

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR1443

Hi

I use IWR1443 and DCA EVM1000 ,mmWavestudio 2.0.1.000.

I manualy set up as follow(I don’t use “Scripts”).

I pushed "DCA1000ARM" buttuon, "Triger Frame"button (Sensor Config) but, adc data is not stored.

On other hand adc data is stored, if I use mmwavestudio1.0.0.0..

I have two question.

1:

Do you know why adc data is not stored?

“Timeout Error! System disconnected” was displayed in the script message

2:

 “xwr12xx_xwr14xx_radarss.bin” and “xwr12xx_xwr14xx_masterss.bin” is correct firmware?

For the firmware to download, refer to the following QA.

http://e2e.ti.com/support/sensors/f/1023/t/858088?tisearch=e2e-sitesearch&keymatch=mmWave%2520studio%25202.1

 

The script message is as follows,

 

[17:24:08] ***Script completed successfully.***

[17:24:10] [RadarAPI]: Opening Gpio Control Port()

[17:24:10] [RadarAPI]: Status: Passed

[17:24:11] [RadarAPI]: Opening Board Control Port()

[17:24:11] [RadarAPI]: Status: Passed

[17:24:12] [RadarAPI]: ar1.FullReset()

[17:24:12] [RadarAPI]: Status: Passed

[17:24:13] [RadarAPI]: Closing Board Control Port()

[17:24:13] [RadarAPI]: Status: Passed

[17:24:13] [RadarAPI]: Closing Gpio Control Port()

[17:24:13] [RadarAPI]: Status: Passed

[17:24:13] [RadarAPI]: ar1.SOPControl(2)

[17:24:13] [RadarAPI]: Status: Passed

[17:24:13] [RadarAPI]: ar1.Connect(19,115200,1000)

[17:24:14] [RadarAPI]: ar1.Calling_IsConnected()

[17:24:16] [RadarAPI]: ar1.SelectChipVersion("AR1243")

[17:24:16] [RadarAPI]: Status: Passed

[17:24:16] [RadarAPI]: ar1.SelectChipVersion("AR1243")

[17:24:16] [RadarAPI]: Status: Passed

[17:24:16] [RadarAPI]: ar1.deviceVariantSelection("XWR1443")

[17:24:16] [RadarAPI]: Status: Passed

[17:24:16] [RadarAPI]: ar1.frequencyBandSelection("77G")

[17:24:16] [RadarAPI]: ar1.SelectChipVersion("XWR1443")

[17:24:16] [RadarAPI]: Status: Passed

[17:24:16] Device Status : XWR1443/QM/SOP:2/ES:3

[17:24:16] [RadarAPI]: ar1.SaveSettings('C:\Users\adws\AppData\Roaming\RSTD\ar1gui.ini')

[17:24:42] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss.bin")

[17:24:42] [RadarAPI]: Downloading BSS Patch RPRC Binary..

[17:24:50] [RadarAPI]: ar1.GetBSSFwVersion()

[17:24:50] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))

[17:24:50] [RadarAPI]: ar1.GetBSSPatchFwVersion()

[17:24:50] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))

[17:25:42] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss.bin")

[17:25:42] [RadarAPI]: Downloading MSS RPRC Binary..

[17:26:01] [RadarAPI]: ar1.GetMSSFwVersion()

[17:26:01] [RadarAPI]: MSSFwVersion:(01.02.05.01 (12/07/19))

[17:26:05] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)

[17:26:05] MSS power up done async event received!

[17:26:05] [RadarAPI]: Status: Passed

[17:26:07] [RadarAPI]: ar1.SelectChipVersion("AR1243")

[17:26:07] [RadarAPI]: Status: Passed

[17:26:07] [RadarAPI]: ar1.SelectChipVersion("XWR1443")

[17:26:07] [RadarAPI]: Status: Passed

[17:26:07] Device Status : XWR1443/QM/SOP:2/ES:3

[17:26:07] [RadarAPI]: ar1.RfEnable()

[17:26:07] BSS power up done async event received!

[17:26:07] [RadarAPI]: Status: Passed

[17:26:08] [RadarAPI]: ar1.GetMSSFwVersion()

[17:26:08] [RadarAPI]: MSSFwVersion:(01.02.05.01 (12/07/19))

[17:26:08] [RadarAPI]: ar1.GetBSSFwVersion()

[17:26:08] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))

[17:26:09] [RadarAPI]: ar1.GetBSSPatchFwVersion()

[17:26:09] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))

[17:26:55] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)

[17:26:55] [RadarAPI]: Status: Passed

[17:26:56] [RadarAPI]: ar1.LPModConfig(0, 0)

[17:26:56] [RadarAPI]: Status: Passed

[17:26:57] [RadarAPI]: ar1.RfInit()

[17:26:57] RF Init async event received!

[17:26:57] [RadarAPI]: Time stamp, Temperture: 50348,33; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 0, 0; RxIQMM Status, Update: 1, 1;

[17:26:57] [RadarAPI]: Status: Passed

[17:27:01] [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)

[17:27:02] [RadarAPI]: Status: Passed

[17:27:02] [RadarAPI]: ar1.LvdsClkConfig(1, 1)

[17:27:03] [RadarAPI]: Status: Passed

[17:27:04] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)

[17:27:04] [RadarAPI]: Status: Passed

[17:27:11] [RadarAPI]: ar1.GetCaptureCardDllVersion()

[17:27:11] [RadarAPI]: Sending dll_version command to DCA1000

[17:27:11] [RadarAPI]:

[17:27:11] DLL Version : 1.0

[17:27:11] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")

[17:27:11] [RadarAPI]: Status: Passed

[17:27:14] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)

[17:27:14] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 1, 1, 2, 3, 30)

[17:27:14] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)

[17:27:14] [RadarAPI]: Sending fpga command to DCA1000

[17:27:14] [RadarAPI]:

[17:27:14] FPGA Configuration command : Success

[17:27:14] [RadarAPI]: Sending record command to DCA1000

[17:27:14] [RadarAPI]:

[17:27:14] Configure Record command : Success

[17:27:14] [RadarAPI]: ar1.GetCaptureCardFPGAVersion()

[17:27:14] [RadarAPI]: Sending fpga_version command to DCA1000

[17:27:14] [RadarAPI]:

[17:27:14]

[17:27:14] FPGA Version : 2.8 [Record]

[17:27:14]

[17:27:18] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)

[17:27:18] [RadarAPI]: Status: Passed

[17:27:19] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0)

[17:27:19] [RadarAPI]: Status: Passed

[17:27:22] Test Source Already Disabled...!!!

[17:27:22] [RadarAPI]: ar1.DisableTestSource(0)

[17:27:22] [RadarAPI]: Status: Passed

[17:27:22] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1)

[17:27:22] [RadarAPI]: Status: Passed

[17:27:24] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)

[17:27:24] [RadarAPI]: Sending start_record command to DCA1000

[17:27:30] [RadarAPI]: ar1.StartFrame()

[17:27:30] [RadarAPI]: Status: Passed

[17:27:30] Frame start async event received!

[17:27:30] [RadarAPI]: Frame Ended

[17:27:34] [RadarAPI]:

[17:27:34] Frame End async event received!

[17:27:34] [RadarAPI]:

[17:27:34] Start Record :

[17:27:34] Timeout Error! System disconnected