This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWAVE-STUDIO: Unable to load DLL in mmWave Studio 2.1.1.0

Part Number: MMWAVE-STUDIO


Hello,

I have been having issues getting the latest version of mmWaveStudio running. Version 2.1.1.0.

  • I've tried re-installing the 32-bit Matlab runtime environment version 8.5.1. As linked to in the user guide documentation.
  • I have FTDI drivers installed
  • MSFT visual C++ 2013 is installed
  • HSDC Pro Software is installed

I've been able to run previous versions of the mmwaveStudio, when it was included with the DFP package.

See the error below:

[14:54:13] Matlab Runtime Engine is installed
[14:54:13] [RadarAPI]: Starting Matlab Engine..
[14:54:13] [RadarAPI]: Error: The type initializer for 'MatlabPostProcGui.MatlabPostProcGUIClass' threw an exception.
[14:54:13] Trace:
[14:54:13] at MatlabPostProcGui.MatlabPostProcGUIClass..ctor()
[14:54:13] at AR1xController.frmAR1Main.InitMatlabPostProcEngine(String PostProcesspath)
[14:54:13] [RadarAPI]: Error: Error occured in Matlab Initialization
[14:54:13] [RadarAPI]: Matlab Engine couldn't be Started..
[14:54:15] [RadarAPI]: ar1.selectCascadeMode(0)
[14:54:15] [RadarAPI]: Status: Passed
[14:54:15] [RadarAPI]: ar1.LoadSettings('[REDACTED]')
[14:54:15] [RadarAPI]: Error: Object reference not set to an instance of an object.
[14:54:15] Trace:
[14:54:15] at AR1xController.ScriptOps.getMatlabPostProcVersion()
[14:54:15]
[14:54:15] &&&&&&&&&&&&&&&&&&&&
[14:54:15] ***Script FAILED!***
[14:54:15] &&&&&&&&&&&&&&&&&&&&
[14:54:15] Exception message is:
[14:54:15] Unable to load DLL 'mclmcrrt8_5_1.dll': The specified module could not be found. (Exception from HRESULT: 0x8007007E)

Thanks,

Erik