This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Regulation in the 60 GHz band

Part Number: IWR6843
Other Parts Discussed in Thread: IWR1642

Hi,

My understanding is IWR6843 can be used for indoor applications without regulatory restrictions (unlike the 77 GHz band which is only meant for automotive and airport use)

Can you please verify? Is there any regulation/compliance related document I should be aware of before committing to 60 GHz band for non-automotive applications?

Regards,

Cagri

  • Hi,

    The regulations changes from region to region, in the US (FCC) there are varying EIRP, TX power, bandwidth limit for various non automotive use case. I recommended confirming the limits for the region based on your use case before going ahead with the design.

    For more on FCC regulation see FCC 15.255, for EU EN 302 729 applies for fluid level sensing and  EN 305 550 some other applications

    Regards,

    Charles O

  • Hi Charles,

    Thank you for the info. I will look at the specs you mentioned as well.

    Just to make sure I understand it correctly, are you going to provide further information on the 60 GHz power restrictions for the US after you hear from your team? If so, I will await your response on that.

    By the way, one thing I observed related to the IWR6843 is its transmit power is 2 dBm lower than its 77 GHz counter part (IWR1642). I presume this reduced level may have something to do with the power restriction you mentioned for the 60 GHz band.

    Regards,

    Cagri

  • Hi,

    We don't have more information to provide on 60GHz restriction at this time. My comment was to determine what your application is and review FCC 15.255 for limits relating to the application.

    The transmit power is stated in the datasheet, IWR162 has a TX power of 12.5dBm and IWR6843 TX power of 12dBm. There may be board to board variation but the TX power for both devices are relatively similar.

    If you have any questions after reviewing the standard please post on the forum.

    Regards,

    Charles O

  • Hi Charles,

    Thank you for the clarification.

    I read the FCC 15.255 for the 60 GHz power limitations. Since I will be focusing on indoor sensing applications, my understanding is the total transmitted power shall not exceed 10 dBm in my case. Since IWR6843 TX power is 12 dBm, a power control is required to be able to work with this part. I had a search on the forum and located the thread below, which you will recognize. It seems power backoff is what I will need to reduce the transmit power.

    By the way one part I could not understand in the below thread is why 3 transmit antennas EACH with 10 dBm output gives an EIRP of 23.7 dBm. If you could clarify that calculation, that will be helpful. If there are additional threads that you think will be helpful for me on this topic (i.e. tx power control, total EIRP power calculation etc.), I would appreciate it if you could share those also.

    Regards,
    Cagri

  • Hi,

    I recommend talking to a TCB about this. The understanding is that for field disturbance sensor, which your use case most likely fall under the limits are 

    1. For 61-61.5GHz Bandwidth, the average power shall not exceed 40 dBm, and the peak power of any emission shall not exceed 43 dBm
    2. Out side of 61-61.5GHz, but widthin 57-71 GHz band,  emissions shall not exceed 10 dBm, and the peak power of any emission shall not exceed 13 dBm.

    the post is adding the TX to antenna gain  (10dBm + 4.7dB for 3 TX + 9dBi for antenna gain == 23.7 dBm)

    see section 5.1 of linked appnote https://www.ti.com/lit/an/spracp3a/spracp3a.pdf

    Regards,

    Charles O

  • Hi Charles,

    Thank you for your note and the pdf guide. These are really helpful.

    Regarding the relevant clause you mentioned, since my application's bandwidth will not only occupy the 500 MHz within the 61.0 - 61.5 GHz band, clause (3) will be relevant I think (I included them below for our reference). The latter part of clause (2) is referring to transmission outside of the actual bandwidth it seems. However, clause (3) covers applications that span a much wider bandwidth than the 500 MHz (mentioned in clause (2) ) 

    I will review the information you shared on the power back off as well and try to digest it in the meantime. I will include additional questions, if any.

    Regards,

    Cagri

    (2) For fixed field disturbance sensors
    that occupy 500 MHz or less of band-
    width and that are contained wholly
    within the frequency band 61.0–61.5
    GHz, the average power of any emis-
    sion, measured during the transmit in-
    terval, shall not exceed 40 dBm, and
    the peak power of any emission shall
    not exceed 43 dBm. In addition, the av-
    erage power of any emission outside of
    the 61.0–61.5 GHz band, measured dur-
    ing the transmit interval, but still
    within the 57–64 GHz band, shall not ex-
    ceed 10 dBm, and the peak power of any
    emission shall not exceed 13 dBm.


    (3) For fixed field disturbance sensors
    other than those operating under the
    provisions of paragraph (b)(2) of this
    section, the peak transmitter con-
    ducted output power shall not exceed
    10 dBm and the peak EIRP level shall
    not exceed 10 dBm.

  • Hi,

    Yes, previous post was inaccurate, for your application clause 3 applies, the peak transmitter conducted output power shall not exceed -10 dBm and the peak EIRP level shall not exceed 10 dBm.

    Correction to the previous post 

    1. For 61-61.5GHz Bandwidth, the average power shall not exceed 40 dBm, and the peak power of any emission shall not exceed 43 dBm
    2. Out side of 61-61.5GHz, but widthin 57-71 GHz band,  emissions shall not exceed 10 dBm, and the peak power of any emission shall not exceed 13 dBm.. the peak transmitter conducted output power shall not exceed -10 dBm and the peak EIRP level shall not exceed 10 dBm.

    Regards,

    Charles O

  • Thanks for the clarification Charles.

    Regards,
    Cagri