Other Parts Discussed in Thread: AWR1843, AWR1243
Hi,
I am using mmWave sensing estimator for estimating chirp parameters.I have few queries:
1) Does radar cube size limitation exist in the case when i am just capturing data from AWR1843 using DCA1000?
2)What is the measurement rate in case of AWR1843?How i can calculate it?
3)I am entring range and velocity parameters (corresponding to the chirp parameters set by me) that doesn't give an error in mmWave studio,but when i enter them here, i am getting errors relating to radar cube size and sampling rate.Why is that?
2) Max range calculation is done using the formula in the attached figure as mentioned in one of the answered questions.What is the quantity Nr?Is it equal to num of TX antennas+num of RX antennas?(6 in case i am using 4RX and 2TX antennas).Can you kindly provide a sample calculation for min SNR of 10dB and RCS of 0.01 square meter for AWR1843?
Thanks