TMUX8108: Maximum frequency for signals passed through?

Part Number: TMUX8108

Tool/software:

Hi,

I am looking to pass a signal (current of about 30mA provided by a voltage controlled Howland Current Pump powered by +/- 30V) from D to Sx (one of S1 to S8).

After selecting one Sx (e.g. Sx)  and wait for the T_ON time, what will the signal maximum frequency I can pass? Or what is the minimum current pulse width I can pass through this mux. and close this pulses can be one to the following one?

Thanks,

Cezar