This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV4051A: SN74LV4051APWR

Part Number: SN74LV4051A

Tool/software:

Hi Team, 

I am looking for DC analysis for this 8:1 mux-  SN74LV4051APWR.
Could you please provide sufficient data including -

VIH(min) (V)
VIL(max) (V)
VOH(min) (V)
VOL(max) (V)


Please provide above details at your earliest convenience.

Thankyou  and regards
Rishabh Khugshal
9310770074
VVDN TECHNOLOGIES 

  • The VIL/VIH limits for the control inputs are specified in the datasheet.

    The I/O pins are not buffered and do not have switching thresholds. This device is an analog switch; a closed switch behaves like a 30 Ω resistor.