Hi
I'm a new user of CCS4. I remember in old CCS versions, we can click "load program" everytime we rebuild it. But in the CC4 version, I could only manually load the program for the first time after I launch TI debugger. After the board is connected, if I rebuild the program, the "load program" will disappear. In stead, it will ask me if I need to re-load the program. Can I set it as manually "load" the program?
in the past my steps: load---observe---power down---debug--rebuild---power up---load---run.....
can I do it the same way in CCS4? I prefer manually load it instead of automatically load.
By the way, how can I load the program only in RAM(i.e, not store in FLASH) so that after the target board reset, I can still have my own original codes?
Thanks,
Violet