This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
All:
I have been using a Windows7 laptop that is win32. If another windows7 laptop is win64, are there any installation issues?
i.e., can the CCS5.2.0.00069_win32.zip be used for a windows7 win64 install?
Hi Todd,
No issues using win7-64. That is my laptop also. CCSv5 is a 32-bit app but it is fully supported on win7-64.
There are a few potential 'gotchas' though. Most revolve around permissions and UAC. For more info, see:
http://processors.wiki.ti.com/index.php/FAQ_-_CCSv5#Operating_System_Support
I have full admin rights to my machine and CCS runs just fine.
ki
HI Todd,
that's what we're here for.
All the best with development.
Best Regards,
Lisa