This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
The CCS installation process is terminated on my win7 OS, I attached the install log. Please have a look.
Thanks.
Allen
Hi Allen,
a couple things from first glance
1 - you seem to be using both a C and D drive. I would not recommend this. I would recommend fully unzipping and installing to a simple local directory like c:/ti or c:/myccs.
2- I would double check for antivirus interference here as well
Please keep us informed.
Best REgards,
Lisa
Hi Allen,
as a next step can we please ask you to double check whether eclipse fully uzipped?
Can you please check the contents of C:/Users/xiluo/AppData/Local/Temp/ijtmp_4F4C7771-4DFA-494C-A256-3683C0EA9CAC, C:/Users/xiluo/AppData/Local/Temp/ijtmp_4F4C7771-4DFA-494C-A256-3683C0EA9CAC/baserepo and C:/Users/xiluo/AppData/Local/Temp/ijtmp_4F4C7771-4DFA-494C-A256-3683C0EA9CAC/eclipse?
The eclipse unzip commands are:
C:/Users/xiluo/AppData/Local/Temp/ijtmp_4F4C7771-4DFA-494C-A256-3683C0EA9CAC/unzip.exe -q -o -d "C:/Users/xiluo/AppData/Local/Temp/ijtmp_4F4C7771-4DFA-494C-A256-3683C0EA9CAC" "C:/CCS5.3.0.00090_win32/baserepo/eclipse_core_3.7.2.zip"
C:/Users/xiluo/AppData/Local/Temp/ijtmp_4F4C7771-4DFA-494C-A256-3683C0EA9CAC/unzip.exe -q -o -d "C:/Users/xiluo/AppData/Local/Temp/ijtmp_4F4C7771-4DFA-494C-A256-3683C0EA9CAC/baserepo" "C:/CCS5.3.0.00090_win32/baserepo/eclipserepo.zip"
Best Regards,
Lisa
Hi Lisa,
If I press "Debug", I will enter the visual studio debug mode which I can see the dis-assembly of setup program. There will pop up a series of dialog box, it's something like:
By the way, I have tried the installation in some other PC, it succeed in one win7-64 OS, but failed in other win7-32 OS and my PC is also win7-64.
But I found that there is one same thing has been done in the two PC which are failed, we have installed CCS5.0.3 in the two PC, but the successful one is clear of this software. So do you think it might be the reason?
I will also try to clear my PC environment and re-install it again, any progress will be posted here. Thanks.
Allen
Hi Allen,
ok, please clean and do try a fresh installation. Although it should not, it is possible a previous install is confusing the installer and making it use "rerun" mode which is not good. Also, as mentioned, please be sure no junctions/mapped or virtual drives are used.
Please keep us informed.
Best Regards,
Lisa
Hi Lisa,
Sorry for the oblivion for update.
Actually, there is no improvement on the issue though I have tried in many ways. My colleague has installed a WIN-XP OS in her VMware virtual machine and try to install 5.3 again, but unexpectedly it's also failed. Then she install v5.2 instead and it works.
It seems the problem might be suspended and please notice me if you see something new about this.
Thanks for any effort.
Allen
HI Allen,
ok, did you try a clean fresh installation removing the previous installations and clearing the isntalljammer folders as well? As mentioned, we think perhaps the multiple attempts was confusing the installer into rerun mode.
Please keep us informed. Also you may want to try the v5.4 beta with its slightly newer installer.
Best Regards,
Lisa