This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I have downloaded CCS5.5.0.00077_win32 and tried to install it on Windows 8 , 64 bit.
First time it gave Failed to install Eclipse error after few seconds. Second time it threw different error.
Attached is the error log. I have purchased a 3 user floating license and I want this system to be the license sever.
Pls check the issue urgently.
Regards
JK
Error in action ExecuteAction Error in action ExecuteAction Error in action ExecuteScript list element in quotes followed by ":" instead of space while executing "::InstallJammer::actions::$component $this" while executing "$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within "::InstallJammer::ExecuteActions $action -parent $id -conditions $eval" (procedure "::InstallJammer::actions::ExecuteAction" line 35) invoked from within "::InstallJammer::actions::$component $this" while executing "$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within "::InstallJammer::ExecuteActions $action -parent $id -conditions $eval" (procedure "::InstallJammer::actions::ExecuteAction" line 35) invoked from within "::InstallJammer::actions::$component $this" Error in action ExecuteAction Error in action ExecuteAction Error in action ExecuteScript list element in quotes followed by ":" instead of space while executing "::InstallJammer::actions::$component $this" while executing "$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within "::InstallJammer::ExecuteActions $action -parent $id -conditions $eval" (procedure "::InstallJammer::actions::ExecuteAction" line 35) invoked from within "::InstallJammer::actions::$component $this" while executing "$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within "::InstallJammer::ExecuteActions $action -parent $id -conditions $eval" (procedure "::InstallJammer::actions::ExecuteAction" line 35) invoked from within "::InstallJammer::actions::$component $this" while executing "$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within "::InstallJammer::ExecuteActions $id -when $when" (procedure "::InstallJammer::RaiseEventHandler" line 93) invoked from within "::InstallJammer::RaiseEventHandler .wizard" (command bound to event)
Hi,
Did you try running in compatibility mode configured as Windows 7?
Also go through this link:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/290318.aspx
Regards,
Gautam
JK,
Would you be able to attach the logs from the InstallJammer folder (C:\Program Files\InstallJammer Registry\ccsv5\<install_random_number>\ )?
JK,
On windows 7, 64-bit, the precise location is C:\Program Files (x86)\InstallJammer Registry\ccsv5\60556FE5-C1A1-4061-8DF8-FFB8393BAE2D. The InstallJammer Registry folder is hidden by default, so you may need to change your folder permissions to see it.
Andy,
Thanks.
Attached is the logs from InstallJammerRegistry. I have tried the following, but no use.
1. Run setup.exe as admin
2. Changed the installation folder.
Best Regards
JK,
I think the problem is probably being caused by your anti-virus program. In addition to the firewall, are you able to temporarily turn off the real time file protection feature?