This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adding "Empty Grace Project" to New CCS Project Wizard for CCS v6

I am using CCS v6.0.1.00040.  I have installed Grace from the Apps Center. The Grace tools are installed into CCS. However, when starting a new CCS Project, the "Empty Grace (MSP430) Project" option is not available.

Question: How do I add this entry into the new project Wizard?

Thanks.

  • I found the answer -- I needed to add -->

    1) in the Target pull-down:  MSP430Gxxx Family

    And 2) the specific micro-Controller in the next pull-down selection.

    After this, the "Empty Grace (MSP430) Project" appeared in the Empty Projects Choices.

    Regards,