OS : Windows 7 - 64bit service pack 1
CCS : v5.1.0.09000
We are using CCS floating server license in our project.
To set up the server followed the steps as mentioned in :
http://processors.wiki.ti.com/index.php/License_Server_Administration_for_CCS#Windows:_graphical_setup
After this we are able to detect and use the floating server license from client PCs.
To use the license from the server PC itself followed the steps as in :
But the CCS IDE in server PC is not able to detect the above mentioned license.
In the first line of "license.txt" file at : C:\Users\<username>\AppData\Local\.TI\213602635\0 tried putting the following combinations :
1. @XXX
2. XXX
where XXX - server computer name.
None seemed to work.
Please support in this regard.