This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What PCs will CC 4.10 (not CCS) run on? I have a customer who needs to revive a C50 project and will need to use that...
FYI, I have a parallel thread with Spectrum Digital and they informed me that XDS510PP Plus will support C50 along with CC 4.10, but it would require true motherboard parallel port, not an adapter.
Brad
I'm thinking from the opposite end of the spectrum. I'm sure it would fail on Vista/7. What about XP? 2000? NT? In other words, what's the most recent OS that I could run CC 4.10 on?
The last computer we (DCAT) had it running on was Windows 98 based, which was only around for specifically running old Code Composer for C3x/4x stuff (now it is gone).
I have heard of customers getting it to mostly work with XP (so NT and 2k may also work somewhat), I am not sure how solidly that is tested though, which probably means you could get some functionality in 7 with XP virtual machine mode, but you never know.
The best advice I could give would be to give it a try and see what happens, and if at all possible convince your customer to use something newer :).