This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Missing driverlib in Project Templates and Examples

Tool/software: Code Composer Studio

I had this issue in CCS 6.x and now CCS 7. When I open a new CCS Project the template for a project that uses the driverlib is missing.

  • Which device family are you working with? Most likely we should be able to point you to a replacement example project that you can start with. 

    Michael Harsh said:
    When I open a new CCS Project the template for a project that uses the driverlib is missing.

    Was this something that was present in earlier versions of CCS (prior to CCSv6)?

  • I do not have the problem with CCSv7