Tool/software: Code Composer Studio
I am using a TI's image processing lib in my project. This is the step while i am using the lib:
Step1:Download the package from the website: http://www.ti.com/tool/sprc264#technicaldocuments(TMS320C6000 Image Library (IMGLIB))
Step2:Install the package into my own direction:D:\TI\imglib_c66x_3_2_0_1
Step3:Create a new Project with a main.c file.
Step4:Modify the command link file. Add the new line like this:
-l "imglib2.l64P"
Step5:Build my project.Add get the error:
After that, I have try another way to use the lib: Set the Project's including path.
The IMGLIB's usersguide tell me to do this!
And then i also set the include path for .h files:
Call the .h file in my project:
#include "stdio.h"
#include "math.h"
#include "stdlib.h"
#include "imglib.h"
int main()
{
printf("Test the IMGLIB\n");
return 0;
}
Build The project:
The imglib.h include the IMG_boundary_16s.h and create the error:
So I want to know how to include the .h file correctly and completely. Is there any UsersGuide for us to Refer! I think that there are so many other libs need to be include into my Project, how can i fix all the questions as you tell me! Thanks a lot!