This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
My CCS has been unable to successfully update the Marketplace Client for over a week, reaching out to see how to complete. Other updates and installs have occurred since then, unsure why this is stuck. When I attempt to install this update I get the following message -
An error occurred while collecting items to be installed
session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,com.sun.jna,4.5.1.v20190425-1842
No repository found containing: osgi.bundle,com.sun.jna.platform,4.5.1.v20190425-1842
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.core,1.7.7.v20190521-1752
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.core.win32,1.7.7.v20190521-1752
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.help.ui,1.7.7.v20190521-1752
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.ui,1.7.7.v20190521-1752
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.ui.css,1.7.7.v20190521-1752
No repository found containing: org.eclipse.update.feature,org.eclipse.epp.mpc,1.7.7.v20190521-1752
See attached for more detailed description. What is the issue here, how can this complete?
I don't think this update is in the default list of Update sites, so I'm not sure how it is showing up for you. However, not installing that update should not impact any CCS functionality. There should be a version of Marketplace Client installed with base CCS, so you can simply disable that update unless you have a specific reason for needing that update.
What does your "Available Software Sites" list look like (under Window->Preferences->Install/Update)? You should be able to disable the site that provides the update for Marketplace Client from there.