This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I try to install ccs 5.5 32 bit, on win7x64 bit.
I try on my computer, and on another one, and on Virtual machine of win7x64 bit.
In all those cases the installation failed in the same point , and with the same error message , that it " cannot continue with the installation due to error"
is it possible to install ccs 32 bit on win 7x 64 bit machine?
Regards.
Asher.
asher bara said:is it possible to install ccs 32 bit on win 7x 64 bit machine?
Yes, the 32-bit version of CCS can be installed and run on 64-bit Windows. However is there a reason you are locked into these older versions of CCS? Note that these old versions are no longer supported, so unless there is a very compelling reason to use them I would strongly recommend upgrading to newer tools.