This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
After a clean install of CCS 9 (latest) on my Linux, it first started ok.
Then, after it pulled updates, CCS said needs to re-launch. After that, I cannot get pass the splash screen, it keeps crashing / getting killed, on some internal segfault.
Tried cleaning all local user ti files, configs, workspaces - nothing.
Worth noting: because this is a 'sudo' type install (effectively as root), this happens for the root user, which you have to use to upgrade / update, and install plugins.
For some strange reason, this error does not appear to manifest or to the same extent, as a 'normal' user - the CCS IDE starts if non-root user starts it.
However, it is still broken now for me as far as I cannot then update / install new plugins , as I need root...
No clue what is going on.. Anyone ?
So far it's been not best experience .. many segfaults errors and crashes while trying to access different parts / functions of CCS
I don't know if this trace can help, most likely not, but this is last thing i see when ltrace'ing the ccstudio binary.
<snip..>
strcat("", "localhost,,127.0.0.0/8,127.0.0.1"...) = "localhost,,127.0.0.0/8,127.0.0.1"...
strstr("localhost,,127.0.0.0/8,127.0.0.1"..., "127.0.0.0/8") = "127.0.0.0/8,127.0.0.1/8"
strstr("localhost,,127.0.0.0/8,127.0.0.1"..., "127.0.0.1/8") = "127.0.0.1/8"
setenv("no_proxy", "localhost,,127.0.0.0/8,127.0.0.1"..., 1) = 0
--- SIGSEGV (Segmentation fault) ---
--- SIGSEGV (Segmentation fault) ---
--- SIGSEGV (Segmentation fault) ---
--- SIGSEGV (Segmentation fault) ---
+++ killed by SIGSEGV +++
bang, spash is gone .. app killed
I had to nuke that install, and restart.
When I re-started the installation binary, pointing to the same installation directory where previous version was installed, the installer told me something along the lines , contains previous installation which is "corrupt" .
So, could that be that the updates that are pushed to the CCS are corrupting Linux install .. ?
After I've re-installed, at least I got back to things working. I do not know what was the original issue, and if it will/not come back again...
(On the side note, default installation file creates few issues. Mostly ones I seen are incorrect / invalid permissions set on files - anything from no executable bits set on *.so files, to executable bits set on normal / plain files, to exec bits set on jars, etc . .. Some directories not executable (cannot change into) by non-owner, etc...
Could be install was created based on Windows files/filesystem.. Also, some SDK packages I've seen get downloaded/installed, and create folders with full read/write access to folders to anyone, in user directory.. This is a bit of a hole for Linux.
Anyone else saw this .. ? I do not trust really that CCS Linux installer )