This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
My problem (as far as I'm knowledgeable) doesn't go much deeper than what the thread title says: whenever I try to launch CCSv8 (either directly or through a shortcut), the splash screen flashes for a split second and then disappears without CCS progressing further in starting up. This is on a completely fresh install (offline install, only selected SimpleLink MSP432), in that I removed all traces of CCS prior to installing it again. This happens whether I run as administrator, or from whatever drive.
I would provide logs if they would help, but I'm not sure where to look for them.
Thanks, Layne
Layne Hoelscher said:Just to further clarify the problem, when it's installed on a USB drive and run on another computer, the program starts and runs normally. Only when I use it on this PC does CCS crash in the way I've described (whether that be from the USB or not).
If I understand correctly, CCS is installed on a USB stick. When plugged into your Windows 10 b1803 machine, it does not run (crash). When you take that same stick and run it from another PC, it runs ok? What is the OS of that PC where it runs fine? Which PC was used to install it on the USB stick?
Thanks
ki
I installed CCSv8 to both the original computer (the one it crashes on) and to the USB stick using the "crashes-on" computer. The build number for the computer that CCSv8 launches fine on (running from the USB install) is also 1803 (Windows 10).