Tool/software: WEBENCH® Design Tools
Please see attached the schematic recommended by the WEBENCH and the schematic we implemented.
On our schematic, please see the STEP-UP REGULATOR and the CURRENT SENSE pages for all pertaining information.
If we short pins 5 and 6 on U7 (ISNS- and ISNS+) the design delivers minimum 4A at 22V on a resistive load.
If we leave the design as is, with 3 mOhm current sense resistor, the voltage output is cut to 12V when the output current is about 0.7A
The design behaves as the current peak in the inductor is 4 times greater than expected.