Hi,
After my IT department installed PSpice for TI on my machine, it has licensing issues (thread PSPICE-FOR-TI: Error LMC-02955). I was told to uninstall it and re-install it. However, there is no windows uninstaller (and no start menu option for launching the program), so my IT department has asked me to get instructions on manually uninstalling it, so that they can try again.
Is removing it as simple as deleting the files at "C:\Cadence\PSpiceTI" and "C:\Users\...\AppData\Roaming\Cadence"?
Couple comments from my IT department:
1) Tell them that your machine has windows customized and many settings are pre-defined by your company.
2) According to what they suggested you to do (to install). I am not sure it will work. Because our computers are set to not allow the user to install anything on this machine, it needs to be installed with the temp admin code.
Any thoughts on the above would be appreciated.
Thanks,
Robbie