This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010059: Regarding Garber file

Part Number: TIDA-010059
Other Parts Discussed in Thread: TIDA-00915

Hi support team.

I have some questions as below.

1) Is it possible to apply TIDA-010059_Power_BoardE1.G1 to the TOP layer instead of TIDA-010059_Power_BoardE1.GBL?
2) If so, is it through-hole connected to the TOP layer TIDA-010059_Power_BoardE1.GTL via the drilled hole TIDA-010059_Power_BoardE1.TX1?
3) In that case, will the BOTTOM layer TIDA-010059_Power_BoardE1.G1 be glued to the aluminum layer?
4) In that case, is the BOTTOM layer TIDA-010059_Power_BoardE1.G1 and the aluminum layer electrically insulated?

Best regards,

Higa